Hi,
From the TRM document, the below describe the functionality OSC1_XO/OSC1_XI
// TRM
OSC1_XO/OSC1_XI — external main crystal interface pins connected to internal oscillator which
sources reference clock. Provides reference clock to PLLs within MAIN domain. This highfrequency oscillator is used to provide audio clock frequencies to MCASPs.
Q) Can OSC1_XO/XI HW be removed if I do not want to use MCASPs?
BR,
Soolim