This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: SDK tune options

Part Number: AM5708

Hi TI Team,

We noticed that for the AM57xx EVM the following TUNE options are configured for the SDK (06 latest): 

TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"

Since the AM5708 uses a single Cortex-A15 (http://www.ti.com/processors/sitara-arm/am5x-cortex-a15/overview.html) we thought in order of performance to use cortex-a15 tune options which resolve for Yocto/open-embedded into:

TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa15"

The problem is that with these TUNE features Valgrind doens't work (output doesn't make sense), further we don't notice any difference. 

Question:
Why do you use the generic armv7 tune options in the SDK rather than the cortex-a15 tune options?

have you considered cortex-a15 tune options or tested with it?