Part Number: TMDSEVM437X
Hello,
Is it possible to use SYSBOOT [01110] - USB MS, EMAC with u-boot 2018 ?
I was trying to use the above boot option, primarily from network along with an USB override.
Unable to get the SPL running properly.
Trial and error method has narrowed down the problem to the following config option
CONFIG_ISW_ENTRY_ADDR=0x40300350
The above option seems to be needed for successful USB Storage booting.
However, network booting fails with the above address.
Is there a way to use one u-boot-spl binary for both USB and ethernet based booting ?
Thanks