We are in the developement of custom board using Dm365. In the Board The Kernel Arago/2.6.31+2.6.32-rc1-r37+gitr Comes up correctly with out any problem.
I used the bin file which i downloaded from http://arago-project.org/files/releases/davinci-psp_3.x.0.0-r37/images/dm365-evm/. But if i compiled the the source code from the same site then it is getting anothe image name and it is not comming up.
Downloaded .bin file
Loading from NAND 512MiB 3,3V 8-bit, offset 0x400000
Image Name: Arago/2.6.31+2.6.32-rc1-r31+gitr
Data Size: 2106356 Bytes = 2 MB
Downloaded Source
Loading from NAND 512MiB 3,3V 8-bit, offset 0x400000
Image Name: Arago-2.6.31
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2106356 Bytes = 2 MB
Can you kindly provide the exact Path to download the Arago/2.6.31+2.6.32-rc1-r31+gitr.