This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3356: DDR CKE questions

Part Number: AM3356

HI,

Our customer is verifying DDR3 with AM3356BZCZ60.
When SI analysis was performed before, all the signal lines were the same, so the same adjustment was done.
However, in order to use low-power mode with AM335x, it is necessary to re-examine the fact that it is necessary to pull-down the CKE signal (e2e.ti.com/.../638781).

Q1.
Only the CKE signal is different from other signals. How do they perform signal validation?
(Can they adjust the amplitude and delay from the CKE waveform?)

Q2.
Is it necessary to make the CKE pattern the same length as other control signals?

Best Regards,

Kouji Nishigata