This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DM3730: DSP, EDMA,L3

Part Number: DM3730

Tool/software: Code Composer Studio

Hi,

I'm facing a L3 in-band error when I use EDMA to copy data from GPMC to SDRAM in DSP.

my processor is DM3730.

this issue occur when DSP code enable a EDMA transfer, and there is no complete callback return, even no error.

check the IVA2.2 system port L3 register, the value is :

L3_IA_COMPONENT : 0x10106331
L3_IA_CORE : 0x200001
L3_IA_AGENT_CONTROL : 0x3e040400
L3_IA_AGENT_STATUS : 0x1000a010
L3_IA_ERROR_LOG :0x84001400
L3_IA_ERROR_LOG_ADDR : 0x0

GEM_AGENT_STATUS : 0x28

EDMA_AGENT_STATUS: 0xa3832

the register value indicate that:

1‘ there is a in-band error in L3_IA_AGENT_STATUS. 

2' EMDA agent is in a request outstanding status.

3' GEM agent is in a waiting response status.

my problem is 

1/ how could be this issue happen? did I need to reduce the L3 bus access?

2/ when this issue happen, what need I do to get the EDMA working right again?

Thanks.