Part Number: AM3359
Other Parts Discussed in Thread: AM3358
Hello,
we are setting up a TCP/IP connection using NDK 2_26_00_08 on a SITARA AM3359.
A ping from an external PC functions well if the PC is located in the same network segment as the AM3359 device, for example AM3359 IP address: 192.168.2.3 and PC 192.168.2.5. But when we try to connect from a different network segment the connection fails.
For example:
SITARA ip address 192.168.1.3 and gateway 192.168.1.1
PC ip address: 192.168.0.5 and gateway 192.168.0.1
Router 1: ip address 192.168.0.0 gateway 192.168.0.1
Router 2: ip address 192.168.1.0 gateway 192.168.1.1
In this case, pinging from the pc to the SITARA only works, after we do a ping from the SITARA to the gateway (192.168.1.1). Without this ping the SITARA cannot be reached from outside the network segement. Do you have any idea why this happens?
Thanks