The AM57xx family has two Gb ethernet ports.
The ports (Port1 and Port2)are connected internally to a switch (GMAC_SW) and the processor transfers data through this switch on Port0.
Can each port be operated simultaneously at the full 1Gbs bandwidth or is the bandwidth halved when both are used at the same time?