Part Number: TMS320C6678
our dsp board use pcie bootmode,it can complete the boot sequnce at most time.THe host is windows 7.but sometimes it couldn't boot up. under this wrong condition,we can download the program through jtag interface,then it will work ok(communicate with pc through pcie interface). I compare the registers under good and bad condition,they have no difference except the PC ,when boot failure,the PC is 0x20bxxxxx,not the cint00 adress.
our power up sequnce is controled by fpga, the control sequence is 1v,1.8v,1.5v,0.75v, reset, por, resetfull in 1ms interval. and assign coresel =8, nmi=1, lreset=1, lresetnmien =1.
Wish someone could help us,thanks!!!