Hi
I am using Linux kernel 4.9.28 on TI AM35xx based custom board presently .
we wish to migrate to new LTS kernel of TI .
as per below 3 links :
http://git.ti.com/ti-linux-kernel/ti-linux-kernel/commits/linux-4.9.y
4.9.191 is latest linux kernel version
http://git.ti.com/ti-linux-kernel/ti-linux-kernel/commits/linux-4.14.y
4.14.142 is latest linux kernel version
http://git.ti.com/ti-linux-kernel/ti-linux-kernel/commits/linux-4.19.y
4.19.71 is latest linux kernel version
since we are using 4.9.28 kernel version now , the closed we see is 4.9.191 to which we plan to move .
we have a question :
Are all TI SOC specific patches equally ported to all 3 LTS kernel 4.9.191 , 4.19.71 , 4.14.142 ?
Do 4.9.191 , 4.19.71 , 4.14.142 kernels have same set of TI SOC specific patches applied to them ?
if so , we can simply move to 4.9.191 which is closet to 4.9.28
Regards
Amit