Other Parts Discussed in Thread: FLASHTOOL
Greetings,
I bought this board from Spectrum Digital a while ago, but did not attempt to use it until today. I setup the hardware as described in the Getting Started Guide.
- Network Connection
- Serial Port Connection
I made sure of the settings on SW7 where as they are supposed to be, set up hyper terminal, connected and powered up the board. I got an error message of the sort: "this is MT...." then a UBL boot failure message that I cannot duplicate anymore because now nothing shows in the terminal window after power is connected. I tried pressing the reset button and cycling power, but the same error remained. I also noticed that the ethernet connector did not have any lights on and that the DS22 LED is flashing green. The LED next to the power connector is green and so are the 7 LED's.
What is going wrong and is there a way I can rectify all this mess? Any ideas?
Thank you,
--
A