Hi,
I am working on the AM65x EVM board with SDK version 06.00.00.07
I have been testing with the classic CAN commands so far and it is working perfectly. But when i tried testing CAN FD using the following command, i got the following error.
Do i need to install some additional module to enable CAN FD? There is no additional command that i found to support CAN FD
Looking for some support here.