Hi Team,
Related on the following request on E2E: https://e2e.ti.com/support/processors/f/791/t/824509
#########################################################################################
We are having trouble running a card we built using the AM3358 CPU from the TI Sitara family.
The debug UART of the card continuously receives 0xC2 information. This information corresponds to an error code. However, we could not find any documents etc. Can you help me with this?
#########################################################################################
I received also the following description:
“We are using Linux v3.2.0. On the zero-generated card, we can't get any signal when it tries to read from Flash (because the flash is empty).
So far, no problems. However, when trying to boot from the SD Card, we receive only 0xC2 signal periodically from the debug port. We don't have a chance to intervene”