Hello,
I got a new PC with Windows 10 and installed TI PinMux Version 4.0.1535. The local and also the TI PinMux tool from the cloud show
Setting up your PinMux Project and a progress bar but do not open my existing *.pinmux files.
These old files start with:
{
"deviceId": "AM5726_SR2.0_beta",
"partId": "ID_500",
"packageId": "ID_0",
"deviceRequirements": {
and end with
"version": "2.0.0"
},
"codeGenOptionsValues": {}
}
Should this work? Is there another possibility to convert the old files for the new PinMux Version?