Part Number: PROCESSOR-SDK-AM65X
Other Parts Discussed in Thread: AM6548
Hi Forum,
I am new to the AM6548 and have never used canutils. Our custom board design is pretty similar to the AM6548 EVM board, and I am using Processor SDK for Linux 06.00.00.07.
Linux boots and I can login as root. What I would like to do is connect simple jumpers with 100 ohm termination resistors to daisy chain can0 to can1. I'd then like to use canutils to send some data from one interface and see that it's received by the other interface, and vice versa.
Can anyone provide a description of how to do this using the provided canutils in the SDK? I confess that I know nothing about these utilities beyond some vague references to "cansend" and "candump". I am also not a Linux expert, so I'm not entirely sure how to start sending from my login console and check for reception using the same console. Do I have to put the sending into the background?
Any examples that you could provide would be extremely welcomed. Thank you for your help; hoping my novice questions will help someone else in need.
Scott