Hello everyone,
I am using EVM320 DM6437 and i try to make a project using C6Flo, but i have some problems....
CCS 3.3 returned me the following 4 Compilation errors. I don't realy undestand what is going on. The only sure is that "dm6437dspapp_1cfg.h" is missing. But why? C6Flo is responsible for generation of this file?
Also what about the message """js: "./dm6437dspapp_1.tcf", line 18: exception from uncaught JavaScript throw: TypeError: Cannot call method "destroy" of undefined (./dm6437dspapp_1.tcf#18)"". ?????
Any idea is welcome
Thanks.
----CCS 3.3 RETURNED THIS-------------------------------------------------------------------------------------------------------------------------------
------------------------- dm6437dspapp_1.pjt - Debug -------------------------
[dm6437dspapp_1.tcf] "C:\CCStudio_v3.3\bios_5_31_02\xdctools\tconf" -b -Dconfig.importPath="C:/CCStudio_v3.3/bios_5_31_02/packages" dm6437dspapp_1.tcf
js: "./dm6437dspapp_1.tcf", line 18: exception from uncaught JavaScript throw: TypeError: Cannot call method "destroy" of undefined (./dm6437dspapp_1.tcf#18)
[dm6437dspapp_1_blocks.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -fr"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/Debug" -i"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1" -i"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/include" -mv6400+ -@"Debug.lkf" "dm6437dspapp_1_blocks.c"
"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/include/dm6437dspapp_1.h", line 7: fatal error: could not open source file "dm6437dspapp_1cfg.h"
1 fatal error detected in the compilation of "dm6437dspapp_1_blocks.c".
Compilation terminated.
>> Compilation failure
[dm6437spapp_1_main.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -fr"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/Debug" -i"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1" -i"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/include" -mv6400+ -@"Debug.lkf" "dm6437dspapp_1_main.c"
"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/include/dm6437dspapp_1.h", line 7: fatal error: could not open source file "dm6437dspapp_1cfg.h"
1 fatal error detected in the compilation of "dm6437dspapp_1_main.c".
Compilation terminated.
>> Compilation failure
[dm6437dspapp_1_threads.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -fr"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/Debug" -i"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1" -i"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/include" -mv6400+ -@"Debug.lkf" "dm6437dspapp_1_threads.c"
"C:/Program Files/Texas Instruments/C6Flo_1.02/work/ProcessFlow1/dm6437dspapp_1/include/dm6437dspapp_1.h", line 7: fatal error: could not open source file "dm6437dspapp_1cfg.h"
1 fatal error detected in the compilation of "dm6437dspapp_1_threads.c".
Compilation terminated.
>> Compilation failure
Build Complete,
4 Errors, 0 Warnings, 0 Remarks.