Part Number: EVMK2GX
Hi,
I would like to booting U-Boot from the emmc.What should I do?
thank you!
Ayden.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EVMK2GX
Hi,
I would like to booting U-Boot from the emmc.What should I do?
thank you!
Ayden.
Hi,
Here is the u-boot users guide:
I suggest you go through the whole u-boot chapter of the Linux Developer's Guide.
Best Regards,
Yordan
Dear Yordan:
Thank you for quick reply.
I have went through the whole u-boot chapter,but I don't get more information about EVMK2GX.In addtion,some commands are not supported,such as bootbus and partconf.Why?
Thank you very much.
Hi,Yordan
I use Processor SDL Linux 06_00_00_07 at 
.What's the difference? but there's not detailed enough to introduction about EVMK2GX board.Do you have any good ideas?
thank you.
Ayden
Hi Ayden,
The procedure for writing MLO & u-boot are described in Section 3.1.1.6.4. Updating an SD card or eMMC with RAW writes in the user guide I've pionted.
The commands which you specify bootbus and partconf are used for dra7xx & am57xx devices, and are not required for k2g u-boot.
Best Regards,
Yordan
Dear ,
According to your instruction,I find some questions as below:
1.After "fatload mmc 0 ${loadaddr} MLO", then the U-boot prompted that 626120 bytes read in 36 ms (16.6 MiB/s).This MLO have 626120 bytes,but the guide indicate "mmc write ${loadaddr} 0x100 0x100",that space size of 256*(block),512 bytes per block usually in emmc.This is not enough space for MLO?
2.the U-boot shown:** Unable to read file rootfs.ext4 **,Atger run fatload mmc 0 ${loadaddr} rootfs.ext4.Before I have used create-sdcard.sh, for create the SD Card using default images from the Processor SDK for Linux.How do I create rootfs.ext4 or find it?
thank you very much.
Ayden.