Other Parts Discussed in Thread: OMAPL138, DAC34SH84, ADS5560
Hello everyone,
I am trying to choose DSP for ultrasound processing. I want to generate and transmit 200 kHz ultrasound signal with transmitting transducer and receive it with receiving one. So far, I have been considering TMS320C6748 DSP Development Kit (LCDK), but considering that it doesn't have integrated DAC and ADC converters I am having trouble deciding which ones to use in order to make them compatible with TMS320C6748 DSP.
Does anybody have suggestions on which ADC and DAC convertors should I pay attention to? Or if another DSP is maybe more suitable?
I am not very experienced in the field of DSPs, therefore I would appreciate any kind of advice or suggestion.
Thanks in advance!