Kemal R. Shakir, hi!
Thanks for the tip: the sdk compilation in Ubuntu version 16 is successful.
But, unlike the previous compilation, linux arago displays a message when it boots:
U-Boot SPL 2018.01-gcdb1cc0a9e (Jun 25 2019 - 11:52:15)
DRA752-GP ES2.0
Trying to boot from MMC1
no pinctrl state for default mode
no pinctrl state for default mode
U-Boot 2018.01-gcdb1cc0a9e (Jun 25 2019 - 11:52:15 +0000)
CPU : DRA752-GP ES2.0
Model: TI AM5728 IDK
Board: AM572x IDK REV 1.3B
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4010496 bytes read in 296 ms (12.9 MiB/s)
101231 bytes read in 74 ms (1.3 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe4000, end 8ffffb6e ... OK
Starting kernel ...
[ 0.000822] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.000831] This ensures that you still see kernel messages. Please
[ 0.000838] update your kernel commandline.
[ 0.001730] /cpus/cpu@0 missing clock-frequency property
[ 0.001748] /cpus/cpu@1 missing clock-frequency property
[ 0.580719] dmi: Firmware registration failed.
[ 1.616246] dra7-pcie 51000000.pcie: phy link never came up
[ 1.806359] cpsw 48484000.ethernet: device node lookup for pps timer failed
[ 1.823502] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_1_8v mode
[ 1.830145] sdhci-omap 4809c000.mmc: no pinctrl state for hs200_1_8v mode
[ 1.960945] omap_voltage_late_init: Voltage driver support not added
[FAILED] Failed to mount POSIX Message Queue File System.
See 'systemctl status dev-mqueue.mount' for details.
[FAILED] Failed to mount Temporary Directory (/tmp).
See 'systemctl status tmp.mount' for details.
[DEPEND] Dependency failed for Network Name Resolution.
[DEPEND] Dependency failed for Network Time Synchronization.
[FAILED] Failed to mount Kernel Configuration File System.
See 'systemctl status sys-kernel-config.mount' for details.
[FAILED] Failed to mount Kernel Debug File System.
See 'systemctl status sys-kernel-debug.mount' for details.
[ OK ] Started Apply Kernel Variables.
[FAILED] Failed to start Remount Root and Kernel File Systems.
See 'systemctl status systemd-remount-fs.service' for details.
[ OK ] Started Journal Service.
Starting Rebuild Hardware Database...
Starting Flush Journal to Persistent Storage...
[ OK ] Reached target System Time Synchronized.
Starting Create System Users...
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Started Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create Static Device Nodes in /dev.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
[FAILED] Failed to mount /media/ram.
See 'systemctl status media-ram.mount' for details.
[DEPEND] Dependency failed for Local File Systems.
[FAILED] Failed to mount /var/volatile.
See 'systemctl status var-volatile.mount' for details.
[DEPEND] Dependency failed for Bind mount volatile /srv.
[DEPEND] Dependency failed for Bind mount volatile /var/spool.
[DEPEND] Dependency failed for Bind mount volatile /var/lib.
[DEPEND] Dependency failed for Bind mount volatile /var/cache.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Reached target Timers.
Starting Network Service...
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Closed Syslog Socket.
[ OK ] Reached target Sockets.
Starting Rebuild Dynamic Linker Cache...
Starting Load/Save Random Seed...
Starting Create Volatile Files and Directories...
[ OK ] Started Emergency Shell.
Starting Rebuild Journal Catalog...
[ OK ] Reached target Emergency Mode.
[ OK ] Started Network Service.
[ OK ] Started Rebuild Hardware Database.
Starting udev Coldplug all Devices...
[ OK ] Reached target Network.
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Rebuild Dynamic Linker Cache.
[ OK ] Started Rebuild Journal Catalog.
Mounting Kernel Configuration File System...
Starting Update is Completed...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[FAILED] Failed to mount Kernel Configuration File System.
See 'systemctl status sys-kernel-config.mount' for details.
[ OK ] Started Update is Completed.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ OK ] Started udev Coldplug all Devices.
You are in emergency mode. After logging in, type "journalctl -xb" to view
system logs, "systemctl reboot" to reboot, "systemctl default" or ^D to boot
into default mode.
Press Enter for maintenance
(or press Control-D to continue):
This - every time the linux arago load.
How to remove it?
Please help.