This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/PROCESSOR-SDK-AM335X: Dual EMAC issue

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3352

Tool/software: TI C/C++ Compiler

Im upgrading my SDK to sdk6.0.7

But when i config dual mac, i used  the 335x-evmsk.dts as reference, and configed the cpsw and emac in dts.

I cannot ping my pc or other network in my am335x filesystem.

The starting information is as following:

------

[ 0.963765] brd: module loaded
[ 0.974173] loop: module loaded
[ 0.979918] libphy: Fixed MDIO Bus: probed
[ 1.054756] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.062463] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
[ 1.070934] libphy: 4a101000.mdio: probed
[ 1.075102] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.084279] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver SMSC LAN8710/LAN8720
[ 1.094451] cpsw 4a100000.ethernet: Detected MACID = 7c:38:66:fb:47:41
[ 1.101303] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.107757] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.113035] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.121136] cpsw 4a100000.ethernet: cpsw: Detected MACID = 7c:38:66:fb:47:43
[ 1.129629] i2c /dev entries driver
[ 1.135126] cpuidle: enable-method property 'ti,am3352' found operations

.....

[ 3.486299] udev[66]: starting version 164
Configuring network interfaces... [ 8.309632] net eth0: initializing cpsw version 1.12 (0)
[ 8.415807] SMSC LAN8710/LAN8720 4a101000.mdio:01: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL)
[ 8.436308] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 8.456409] net eth1: initializing cpsw version 1.12 (0)
[ 8.565940] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
[ 8.581517] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
done.

...

[ 9.755237] random: crng init done
[ 12.566035] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 12.604850] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

------------

Seems that the emac0 and emac1 has been inited ok. However, i cannot ping my pc. The ifconfig result:

eth0 Link encap:Ethernet HWaddr 7C:38:66:FB:47:41
inet addr:192.168.3.11 Bcast:192.168.3.255 Mask:255.255.255.0
inet6 addr: fe80::7e38:66ff:fefb:4741/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:35 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:2402 (2.3 KiB)
Interrupt:41

eth1 Link encap:Ethernet HWaddr 7C:38:66:FB:47:43
inet addr:192.168.4.11 Bcast:192.168.4.255 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:393 errors:0 dropped:0 overruns:0 frame:0
TX packets:393 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:26402 (25.7 KiB) TX bytes:26402 (25.7 KiB)

There a difference in hardware between the demo board and my board. Rmii1 and rmii2 address  are 1,0 instead of 0,1.So i changged the dts emac phy_id.

My pinmux of rmii is:

[MDIO_CLK/TIMER5/UART5_TXD/UART3_RTSN/MMC0_SDWP/MMC1_CLK/MMC2_CLK/GPIO0_1] MDIO_CLK PHY
[MDIO_DATA/TIMER6/UART5_RXD/UART3_CTSN/MMC0_SDCD/MMC1_CMD/MMC2_CMD/GPIO0_0] MDIO_DATA
[XDMA_EVENT_INTR1//TCLKIN/CLKOUT2/TIMER7/PR1_PRU0_PRU_R31_16/EMU3/GPIO0_20] ETH_RST_GPIO0_20 ETH_RST
[GMII1_CRS/RMII1_CRS_DV/SPI1_D0/I2C1_SDA/MCASP1_ACLKX/UART5_CTSN/UART2_RXD/GPIO3_1] RMII1_CRS_DV RMII1
[GMII1_RXERR/RMII1_RXERR/SPI1_D1/I2C1_SCL/MCASP1_FSX/UART5_RTSN/UART2_TXD/GPIO3_2] RMII1_RXERR
[GMII1_TXEN/RMII1_TXEN/RGMII1_TCTL/TIMER4/MCASP1_AXR0/EQEP0_INDEX/MMC2_CMD/GPIO3_3] RMII1_TXEN
[GMII1_TXD0/RMII1_TXD0/RGMII1_TD0/MCASP1_AXR2/MCASP1_ACLKR/EQEP0B_IN/MMC1_CLK/GPIO0_28] RMII1_TXD0
[GMII1_TXD1/RMII1_TXD1/RGMII1_TD1/MCASP1_FSR/MCASP1_AXR1/EQEP0A_IN/MMC1_CMD/GPIO0_21] RMII1_TXD1
[GMII1_RXD0/RMII1_RXD0/RGMII1_RD0/MCASP1_AHCLKX/MCASP1_AHCLKR/MCASP1_ACLKR/MCASP0_AXR3/GPIO2_21] RMII1_RXD0
[GMII1_RXD1/RMII1_RXD1/RGMII1_RD1/MCASP1_AXR3/MCASP1_FSR/EQEP0_STROBE/MMC2_CLK/GPIO2_20] RMII1_RXD1
[RMII1_REFCLK/XDMA_EVENT_INTR2/SPI1_CS0/UART5_TXD/MCASP1_AXR3/MMC0_POW/MCASP1_AHCLKX/GPIO0_29] RMII1_REFCLK
[MCASP0_FSX/EHRPWM0B//SPI1_D0/MMC1_SDCD/PR1_PRU0_PRU_R30_1/PR1_PRU0_PRU_R31_1/GPIO3_15] ETH2_INT_GPIO3_15
[GPMC_A4/GMII2_TXD1/RGMII2_TD1/RMII2_TXD1/GPMC_A20/PR1_MII1_TXD0/EQEP1A_IN/GPIO1_20] RMII2_TXD1 RMII2
[GPMC_A5/GMII2_TXD0/RGMII2_TD0/RMII2_TXD0/GPMC_A21/PR1_MII1_RXD3/EQEP1B_IN/GPIO1_21] RMII2_TXD0
[GPMC_A10/GMII2_RXD1/RGMII2_RD1/RMII2_RXD1/GPMC_A26/PR1_MII1_RXDV/MCASP0_AXR0/GPIO1_26] RMII2_RXD1
[GPMC_A11/GMII2_RXD0/RGMII2_RD0/RMII2_RXD0/GPMC_A27/PR1_MII1_RXER/MCASP0_AXR1/GPIO1_27] RMII2_RXD0
[GPMC_A9/GMII2_RXD2/RGMII2_RD2/MMC2_DAT7/GPMC_A25/PR1_MII_MR1_CLK/MCASP0_FSX/RMII2_CRS_DV/GPIO1_25] RMII2_CRS_DV
[GPMC_WPN/GMII2_RXERR/GPMC_CSN5/RMII2_RXERR/MMC2_SDCD/PR1_MII1_TXEN/UART4_TXD/GPIO0_31] RMII2_RXERR
[GPMC_A0/GMII2_TXEN/RGMII2_TCTL/RMII2_TXEN/GPMC_A16/PR1_MII_MT1_CLK/EHRPWM1_TRIPZONE_INPUT/GPIO1_16] RMII2_TXEN
[GMII1_COL/RMII2_REFCLK/SPI1_SCLK/UART5_RXD/MCASP1_AXR2/MMC2_DAT3/MCASP0_AXR2/GPIO3_0] RMII2_REFCLK
[GPMC_CSN2/GPMC_BE1N/MMC1_CMD/GPIO1_31] ETH2_PHY_INTn_GPIO1-31

My dts about cpsw is as following:

cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
AM33XX_IOPAD(0x914, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
AM33XX_IOPAD(0x918, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
AM33XX_IOPAD(0x91c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
AM33XX_IOPAD(0x920, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
AM33XX_IOPAD(0x924, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
AM33XX_IOPAD(0x928, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
AM33XX_IOPAD(0x92c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
AM33XX_IOPAD(0x930, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
AM33XX_IOPAD(0x934, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
AM33XX_IOPAD(0x938, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
AM33XX_IOPAD(0x93c, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
AM33XX_IOPAD(0x940, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */

/* Slave 2 */
AM33XX_IOPAD(0x840, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a0.rgmii2_tctl */
AM33XX_IOPAD(0x844, PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a1.rgmii2_rctl */
AM33XX_IOPAD(0x848, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a2.rgmii2_td3 */
AM33XX_IOPAD(0x84c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a3.rgmii2_td2 */
AM33XX_IOPAD(0x850, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a4.rgmii2_td1 */
AM33XX_IOPAD(0x854, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a5.rgmii2_td0 */
AM33XX_IOPAD(0x858, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a6.rgmii2_tclk */
AM33XX_IOPAD(0x85c, PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a7.rgmii2_rclk */
AM33XX_IOPAD(0x860, PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a8.rgmii2_rd3 */
AM33XX_IOPAD(0x864, PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a9.rgmii2_rd2 */
AM33XX_IOPAD(0x868, PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a10.rgmii2_rd1 */
AM33XX_IOPAD(0x86c, PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a11.rgmii2_rd0 */
>;
};

&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
dual_emac = <1>;
status = "okay";
};

&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};

&cpsw_emac0 {
phy_id = <&davinci_mdio>, <1>;
phy-mode = "rmii";
dual_emac_res_vlan = <1>;
};

&cpsw_emac1 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "rmii";
dual_emac_res_vlan = <2>;
};

&phy_sel {
rmii-clock-ext;
};

Any fault here?Thank you.

  • Please follow this checklist and post the required information here: processors.wiki.ti.com/.../5x_CPSW

  • iv seen that and above output shows link detection is right. I didn't get any packet with wireshark when i ping my pc.


  • Hi,

    Could you please attach the results of the ethtool -S eth0 after rebooting the board and only bringing up eth0 by itself? Are the IP addresses obtained by DHCP or are they set up statically?

    Best Regards,

    Schuyler

  • I used the arago-base filesystem for test. And i use ifconfig eth0 192.168.3.11 to config the ip  statically. The ethtool result:
    root@am335x-evm:~# ethtool eth0
    Settings for eth0:
    Supported ports: [ TP MII ]
    Supported link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    Supported pause frame use: Symmetric Receive-only
    Supports auto-negotiation: Yes
    Supported FEC modes: Not reported
    Advertised link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    Advertised pause frame use: No
    Advertised auto-negotiation: Yes
    Advertised FEC modes: Not reported
    Link partner advertised link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    Link partner advertised pause frame use: Symmetric Receive-only
    Link partner advertised auto-negotiation: Yes
    Link partner advertised FEC modes: Not reported
    Speed: 100Mb/s
    Duplex: Full
    Port: MII
    PHYAD: 1
    Transceiver: internal
    Auto-negotiation: on
    Supports Wake-on: d
    Wake-on: d
    Current message level: 0x00000000 (0)

    root@am335x-evm:~# ethtool -S eth0
    NIC statistics:
    Good Rx Frames: 0
    Broadcast Rx Frames: 0
    Multicast Rx Frames: 0
    Pause Rx Frames: 0
    Rx CRC Errors: 0
    Rx Align/Code Errors: 0
    Oversize Rx Frames: 0
    Rx Jabbers: 0
    Undersize (Short) Rx Frames: 0
    Rx Fragments: 0
    Rx Octets: 0
    Good Tx Frames: 107
    Broadcast Tx Frames: 33
    Multicast Tx Frames: 74
    Pause Tx Frames: 0
    Deferred Tx Frames: 0
    Collisions: 0
    Single Collision Tx Frames: 0
    Multiple Collision Tx Frames: 0
    Excessive Collisions: 0
    Late Collisions: 0
    Tx Underrun: 0
    Carrier Sense Errors: 0
    Tx Octets: 16423
    Rx + Tx 64 Octet Frames: 0
    Rx + Tx 65-127 Octet Frames: 80
    Rx + Tx 128-255 Octet Frames: 0
    Rx + Tx 256-511 Octet Frames: 27
    Rx + Tx 512-1023 Octet Frames: 0
    Rx + Tx 1024-Up Octet Frames: 0
    Net Octets: 16423
    Rx Start of Frame Overruns: 0
    Rx Middle of Frame Overruns: 0
    Rx DMA Overruns: 0
    Rx DMA chan 0: head_enqueue: 1
    Rx DMA chan 0: tail_enqueue: 127
    Rx DMA chan 0: pad_enqueue: 0
    Rx DMA chan 0: misqueued: 0
    Rx DMA chan 0: desc_alloc_fail: 0
    Rx DMA chan 0: pad_alloc_fail: 0
    Rx DMA chan 0: runt_receive_buf: 0
    Rx DMA chan 0: runt_transmit_bu: 0
    Rx DMA chan 0: empty_dequeue: 0
    Rx DMA chan 0: busy_dequeue: 0
    Rx DMA chan 0: good_dequeue: 0
    Rx DMA chan 0: requeue: 0
    Rx DMA chan 0: teardown_dequeue: 0
    Tx DMA chan 0: head_enqueue: 107
    Tx DMA chan 0: tail_enqueue: 0
    Tx DMA chan 0: pad_enqueue: 0
    Tx DMA chan 0: misqueued: 0
    Tx DMA chan 0: desc_alloc_fail: 0
    Tx DMA chan 0: pad_alloc_fail: 0
    Tx DMA chan 0: runt_receive_buf: 0
    Tx DMA chan 0: runt_transmit_bu: 8
    Tx DMA chan 0: empty_dequeue: 107
    Tx DMA chan 0: busy_dequeue: 0
    Tx DMA chan 0: good_dequeue: 107
    Tx DMA chan 0: requeue: 0
    Tx DMA chan 0: teardown_dequeue: 0

  • i have checked my dts in pinmux. I found that the default pinmux is for  rgmii and i used it for rmii.

    i use pinmux-tool for the rmii pinmux config and solved the problem. My eth0 could run without any problem right now.

    However, i still don't know why uboot's eth0 could run with the wrong config.