Part Number: TDA2E
Other Parts Discussed in Thread: TDA2
Hello,
1 . dataFormat is showing as SYSTEM_DF_BAYER_BGGR (Not sure what this means)2 . The cmdHeader looks ok, Here the data size is correct x*y*16(Rx Channels)*8(Real & Imag of each 32 bits)
cmdHeader struct <unnamed> {numBuf=1,header=0,payloadType=8,chNum=0,dataSize=16777216...} 0x8621C8F0numBuf unsigned int 1 0x8621C8F0header unsigned int 0 0x8621C8F4payloadType unsigned int 8 0x8621C8F8chNum unsigned int 0 0x8621C8FCdataSize unsigned int x*y*16*4*2 0x8621C900width unsigned int 2048 0x8621C904height unsigned int 256 0x8621C908pitch unsigned int[2] [16384,16384] 0x8621C90C[0] unsigned int 16384 0x8621C90C[1] unsigned int 16384 0x8621C910
3 . Than in NetworkTxLink_drvWriteHeader when we tries to write Network_write in line number 207 than network_rx.exe throws the above mentioned error.
4. Afterwards in the NetworkTxLink_drvSendData line 532 i saw ack = 255 and than status was set to SYSTEM_LINK_STATUS_EFAIL in line 534.
I guess the network_rx.exe cannot handle the packet where the header says packet size is more than 1920*1080*2. So i tried to compile a new network_rx.exe and followed the steps mentioned in section 1.1 of VisionSDK_UserGuide_NetworkTools.docx and then run "gmake Makefile all" and it crashes
c:/CodeBlocks/MinGW/bin/gcc -c -Wall -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build/../common/inc -I../inc -I../priv -I. -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/ti_components/networking/nsp_gmacsw_4_16_01_01/packages -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build/../common/inc -I../inc -I../priv -I. -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/ti_components/networking/nsp_gmacsw_4_16_01_01/packages network_cons_main.c network_cons_thr_win32.c -M > MAKEFILE.DEPEND
make[4]: Leaving directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/network_cons/src'
make[3]: Leaving directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build'
make[2]: Leaving directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build'
"C:/Program Files (x86)/GnuWin32/bin/make.exe" libs
make[2]: Entering directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build'
"C:/Program Files (x86)/GnuWin32/bin/make.exe" -fMAKEFILE.MK -CC:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build/../common/src MODULE=common
make[3]: Entering directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/common/src'
common: Compiling network_api.c
c:/CodeBlocks/MinGW/bin/gcc -c -Wall -O3 -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build/../common/inc -I../inc -I../priv -I. -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/ti_components/networking/nsp_gmacsw_4_16_01_01/packages -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build/../common/inc -I../inc -I../priv -I. -IC:/PROCESSOR_SDK_RADAR_03_07_00_00/ti_components/networking/nsp_gmacsw_4_16_01_01/packages -oC:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build/../lib/obj/common//network_api.o network_api.c
make[3]: *** [network_api.o] Error 1
make[3]: Leaving directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/common/src'
make[2]: *** [libs] Error 2
make[2]: Leaving directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build'
make[1]: *** [exe] Error 2
make[1]: Leaving directory `C:/PROCESSOR_SDK_RADAR_03_07_00_00/vision_sdk/apps/tools/network_tools/build'
gmake: *** [Makefile:27: all] Error 2
Also i see one popup coming up