This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: TDA3X/VISION SDK :- Use case for capture image through CSI and CAL and display on HDMI

Part Number: TDA3XEVM
Other Parts Discussed in Thread: DS90UB960-Q1, TIDA-01004

Hi 

I have got TDA3X EVM board.

I have Adapter board DS90UB960-Q1.- deserializer board

I have TIDA01004 . (Serailzer and camera module.)

I need to have a demo where I want to capture image through TIDA01004 through serializer and then deserializer and recieve image via cAL module and display image as HDMI out.

Capture:-

camera sensor->TIDA01004 serializer->DS90UB960 Dserializer->CSIPHY->CAL module(TDA3)

Display:-

HDMI OUT

Which is the use case which I should  use from the one which is provided in "PROCESSOR_SDK_VISION_03_06_00_00\vision_sdk\apps\src\rtos\usecases folder".

I am looking for use case which close to above mentioned application. I hope as all these boards are from Texas I will have a readymade usecase to support these chips.