I'm sure this is a simple question for those in the know but I'm new to configuring / building linux kernels. I have the OMAPL-138 experimenter kit and DVSDK 4. I am able to build linux from the $DVSDK directory by entering "make linux". This builds a default configuration of linux which I am able to boot from. In my attempt to reconfigure the kernel I do the following:
- from $DVSDK/psp/linux-2.6xxxxx make menuconfig
I make the changes I want (just removing the bootup logo for now). I look at the .config file and it has been modified as expected.
- from $DVSDK I modify the Makefile to NOT use the default config file by commenting out the following line at the top: DEFAULT_LINUXKERNEL_CONFIG=da850_omapl138_defconfig
My thought is that the new .config that was just created would be used instead of the da850_omapl138_defconfig file.
- from $DVSDK make linux
This then executes scripts/kconfig/conf -s arch/arm/Kconfig which displays the following:
*
* Restart config....
* System Type
*
MMU-based Paged Memory Management Support (MMU) [Y/n/?] y
ARM system type
1. Agilent AAEC-2000 based (ARCH_AAEC2000) (NEW)
2. ARM Ltd. Integrator family (ARCH_INTEGRATOR) (NEW)
3. ARM Ltd. RealView family (ARCH_REALVIEW) (NEW)
> 4. ARM Ltd. Versatile family (ARCH_VERSATILE) (NEW)
5. Atmel AT91 (ARCH_AT91) (NEW)
6. Cirrus Logic CLPS711x/EP721x-based (ARCH_CLPS711X) (NEW)