Part Number: TI-PLC-G3-DC
Hi,
There is a front end application with G3 DC that requires multi-screen. In the past, screens are driven by a x86 PC. Now I'm trying to move the business logic and G3 DC to AM5708 so as to replace AM3359 and the huge x86 motherboard. I thought this was easy due to the similar micro-architecture between AM5708 and AM3359. However, g3_dc_AM335X_aes_msb_loadng.exe exit unexpectedly with a segment fault. I consulted my local technical support of TI about it. They advice me to recompile the code in AM5708's environment. I remember another TI's staff has told me that I can apply for special version of G3 DC included the source of G3 DC runing on AM3359 if there is really a demand when I once complain to him about the size of extra x86 board. I have no idea where to send this request so I write this thread. Besides, I don't know which forum should I post this thread. If I had post it to a wrong forum, please help me correct it.
Currently I'm working with G3_DC_SDK_Package_V45010 and it contains the listed code except g3_dc_AM335X_aes_msb_loadng.exe and g3dc_cli_AM335X. I would like to request the special version containing code of g3_dc_AM335X_aes_msb_loadng.exe and g3dc_cli_AM335X.