This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 ISP CCDC problem



//------------------------------call_isp.c---------------------
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <unistd.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <fcntl.h>
#include <sys/mman.h>
#include <linux/fb.h>
#include <sys/socket.h>
#include <asm/types.h>
#include <linux/netlink.h>


#define FRAME_BUFF_SZ   512*512//672*480
int file;

int main(void)
{
        int video;
        int contrast,bright;
        int i;
        char *pbuff = NULL;
        char AppBuf[512*512];

        system("busybox-omap rmmod  isp.ko");
        system("busybox-omap insmod  ./isp.ko"); 
        file= open ("/dev/isp", O_RDWR);
        if(file<0)
        {
                printf("Open driver faile\n");
        }              
       
        while(1)
        {       
                read(file, AppBuf, 512*512);
//                printf("AppBuf[400]=%02X\n",AppBuf[400]);
        }
               
   
        close (file);            
     
}

//-----------------------------call_isp.c---end------------------

 

//-----------------------------isp.c-------------------------------------------------
/* This is the OMAP35xx Camera ISP Driver used for F60plus.
 * We drop the V4L2 (Video for Linux 2) method, we only use
 * the simply way of configuring the registers to let the camera
 * port receive the data from FPGA.
 */
#include <linux/fs.h>  
#include <linux/sched.h> 
#include <linux/kernel.h>
#include <linux/errno.h>
#include <linux/init.h>
#include <linux/slab.h>
#include <linux/module.h>
#include <linux/kref.h>
#include <asm/uaccess.h>
#include <asm/irq.h>
#include <linux/delay.h>
#include <linux/interrupt.h>
#include <linux/version.h>
#include <linux/platform_device.h>
#include <linux/clk.h>
#include <linux/io.h>
#include <linux/module.h>
#include <linux/err.h>
#include <linux/clk.h>
#include <asm/scatterlist.h>
#include <asm/mach-types.h>
//#include <asm/arch/clock.h>  
#include <linux/device.h>
#include <mach/hardware.h>
#include <linux/fb.h>
#include <linux/dma-mapping.h>
#include <linux/vmalloc.h>
#include <linux/mm.h>
#include <linux/device.h>
#include <mach/display.h>
//#include <mach/omapfb.h>
//#include "capture.h"
#include "Capture.h"
#include "isp.h"

//int isp_major = 0;
#define CAMERA_ISP_MAJOR 232      //define the major number of the device

#define VM_RESERVED 0x00080000 /* Count as reserved_vm like IO */

#define CAPTURE_NAME "omap35xxCapture"

typedef char cam_isp_dev_t;
static cam_isp_dev_t cam_isp_devices[257];

static wait_queue_head_t w_queue;
//static int w_flag = 0;

static unsigned char * CptDataBuf __attribute__ ((aligned(32)));
static unsigned char * CptDataBuf_phy __attribute__ ((aligned(32)));
static int xieyuTag;


static void isp_clk_config(void)
{
  omap_writel(EN_CSI2(0) | EN_CAM(1), CM_FCLKEN_CAM);
  omap_writel(EN_CAM(1), CM_ICLKEN_CAM);
  omap_writel(ST_CAM(1), CM_IDLEST_CAM);
  omap_writel(AUTO_CAM(1), CM_AUTOIDLE_CAM);
  omap_writel(0x3, CM_CLKSEL_CAM);
  omap_writel(EN_MPU(1), CM_SLEEPDEP_CAM);
  omap_writel(CLKTRCTRL_CAM(3), CM_CLKSTCTRL_CAM);
  omap_writel(CLKACTIVITY_CAM(1), CM_CLKSTST_CAM);
  omap_writel(POWERSTATE(3), PM_PWSTCTRL_CAM);
  omap_writel(LASTPOWERSTATEENTERED(3), PM_PREPWSTST_CAM);
  omap_writel( EN_WKUP(1) | EN_IVA2(1) | EN_MPU(1), PM_WKDEP_CAM );
  omap_writel( COREDOMAINWKUP_RST(1) | DOMAINWKUP_RST(1) | GLOBALWARM_RST(1) | GLOBALCOLD_RST(1), RM_RSTST_CAM );
 
  ////printk("RM_RSTST_CAM = 0x%x\n",omap_readl(RM_RSTST_CAM));
  ////printk("PM_WKDEP_CAM = 0x%x\n",omap_readl(PM_WKDEP_CAM));
  ////printk("PM_PWSTCTRL_CAM = 0x%x\n",omap_readl(PM_PWSTCTRL_CAM));
  ////printk("PM_PWSTST_CAM = 0x%x\n",omap_readl(PM_PWSTST_CAM));
  ////printk("PM_PREPWSTST_CAM = 0x%x\n",omap_readl(PM_PREPWSTST_CAM));
  ////printk("CM_FCLKEN_CAM = 0x%x\n",omap_readl(CM_FCLKEN_CAM));
  ////printk("CM_ICLKEN_CAM = 0x%x\n",omap_readl(CM_ICLKEN_CAM));
  ////printk("CM_IDLEST_CAM = 0x%x\n",omap_readl(CM_IDLEST_CAM));
  ////printk("CM_AUTOIDLE_CAM = 0x%x\n",omap_readl(CM_AUTOIDLE_CAM));
  ////printk("CM_CLKSEL_CAM = 0x%x\n",omap_readl(CM_CLKSEL_CAM));
  ////printk("CM_SLEEPDEP_CAM = 0x%x\n",omap_readl(CM_SLEEPDEP_CAM));
  ////printk("CM_CLKSTCTRL_CAM = 0x%x\n",omap_readl(CM_CLKSTCTRL_CAM));
  ////printk("CM_CLKSTST_CAM = 0x%x\n",omap_readl(CM_CLKSTST_CAM));
}

static void isp_pin_config(void)
{
  unsigned int data;
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_HS);
  ////printk("CONTROL_PADCONF_CAM_HS = 0x%x \n", data);
  omap_writel(0x12181218, ISP_CONTROL_PADCONF_CAM_HS);
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_HS);
  ////printk("CONTROL_PADCONF_CAM_HS = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_XCLKA);
  ////printk("CONTROL_PADCONF_CAM_XCLKA = 0x%x \n", data);
 
  omap_writel(0x3f181718, ISP_CONTROL_PADCONF_CAM_XCLKA);
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_XCLKA);
  ////printk("CONTROL_PADCONF_CAM_XCLKA = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_FLD);
  ////printk("CONTROL_PADCONF_CAM_FLD = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_D1);
  ////printk("CONTROL_PADCONF_CAM_D1 = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_D3);
  ////printk("CONTROL_PADCONF_CAM_D3 = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_D5);
  ////printk("CONTROL_PADCONF_CAM_D5 = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_D7);
  ////printk("CONTROL_PADCONF_CAM_D7 = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_D9);
  ////printk("CONTROL_PADCONF_CAM_D9 = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_D11);
  ////printk("CONTROL_PADCONF_CAM_D11 = 0x%x \n", data);
 
  data = omap_readl(ISP_CONTROL_PADCONF_CAM_WEN);
  ////printk("CONTROL_PADCONF_CAM_WEN = 0x%x \n", data);
}

static void isp_timing_config(void)
{
  //unsigned int data;
 
  omap_writel(GRESETDIR(1) | DIVC(2) | DIVA(7), ISP_TCTRL_CTRL);
  omap_writel(HS_VS_IRQ(1)              |            
              SEC_ERR_IRQ(1)            |
              OCP_ERR_IRQ(1)            |
              MMU_ERR_IRQ(1)            |        
              OVF_IRQ(1)                |        
              RSZ_DONE_IRQ(1)           |        
              CBUFF_IRQ(1)              |        
              PRV_DONE_IRQ(1)           |        
              CCDC_LSC_PREFETCH_ERRO(1) |
              CCDC_LSC_DONE(1)          |      
              HIST_DONE_IRQ(1)          |      
              H3A_AWB_DONE_IRQ(1)       |    
              H3A_AF_DONE_IRQ(1)        |    
              CCDC_ERR_IRQ(1)           |    
              CCDC_VD2_IRQ(1)           |    
              CCDC_VD1_IRQ(1)           |    
              CCDC_VD0_IRQ(1)
              ,ISP_IRQ0STATUS);
            
  omap_writel(HS_VS_IRQ(1)              |                              
              SEC_ERR_IRQ(0)            |        
              OCP_ERR_IRQ(0)            |        
              MMU_ERR_IRQ(0)            |        
              OVF_IRQ(0)                |        
              RSZ_DONE_IRQ(0)           |        
              CBUFF_IRQ(0)              |        
              PRV_DONE_IRQ(0)           |        
              CCDC_LSC_PREFETCH_ERRO(0) |
              CCDC_LSC_DONE(0)          |      
              HIST_DONE_IRQ(0)          |      
              H3A_AWB_DONE_IRQ(0)       |    
              H3A_AF_DONE_IRQ(0)        |    
              CCDC_ERR_IRQ(0)           |    
              CCDC_VD2_IRQ(0)           |    
              CCDC_VD1_IRQ(0)           |    
              CCDC_VD0_IRQ(0)                  
              ,ISP_IRQ0ENABLE);
  omap_writel(0x0,ISP_TCTRL_FRAME);
  omap_writel(0x0,ISP_TCTRL_PSTRB_DELAY);
  omap_writel(0x0,ISP_TCTRL_STRB_DELAY);
  omap_writel(0x0,ISP_TCTRL_SHUT_DELAY);
  omap_writel(0x0,ISP_TCTRL_PSTRB_LENGTH);
  omap_writel(0x0,ISP_TCTRL_STRB_LENGTH);
  omap_writel(0x0,ISP_TCTRL_SHUT_LENGTH);
  
  ////printk("ISP_TCTRL_CTRL = 0x%x \n", omap_readl(ISP_TCTRL_CTRL) );
  ////printk("ISP_IRQ0ENABLE = 0x%x \n", omap_readl(ISP_IRQ0ENABLE) );
  ////printk("ISP_IRQ1ENABLE = 0x%x \n", omap_readl(ISP_IRQ1ENABLE) );
  ////printk("ISP_TCTRL_FRAME = 0x%x \n", omap_readl(ISP_TCTRL_FRAME) );
  ////printk("ISP_TCTRL_PSTRB_DELAY = 0x%x \n", omap_readl(ISP_TCTRL_PSTRB_DELAY) );
  ////printk("ISP_TCTRL_SHUT_DELAY = 0x%x \n", omap_readl(ISP_TCTRL_SHUT_DELAY) );
  ////printk("ISP_TCTRL_PSTRB_LENGTH = 0x%x \n", omap_readl(ISP_TCTRL_PSTRB_LENGTH) );
  ////printk("ISP_TCTRL_SHUT_LENGTH = 0x%x \n", omap_readl(ISP_TCTRL_SHUT_LENGTH) );
  ////printk("ISP_PING_PONG_ADDR = 0x%x \n", omap_readl(ISP_PING_PONG_ADDR) );
  ////printk("ISP_PING_PONG_MEM_RANGE = 0x%x \n", omap_readl(ISP_PING_PONG_MEM_RANGE) );
  ////printk("ISP_PING_PONG_BUF_SIZE = 0x%x \n", omap_readl(ISP_PING_PONG_BUF_SIZE) );
}

static void isp_BridgeLane_config(void)
{
  unsigned int data;
  /***** ISP_CTRL  */
  omap_writel(FLUSH(0)             |
              JPEG_FLUSH(0)        |
              CCDC_WEN_POL(1)      |
              SBL_SHARED_RPORTB(0) | 
              SBL_AUTOIDLE(1)      | 
              SBL_WR0_RAM_EN(0)    |
              SBL_WR1_RAM_EN(0)    |
              SBL_RD_RAM_EN(1)     |
              PREV_RAM_EN(0)       |
              CCDC_RAM_EN(0)       | 
              SYNC_DETECT(0x3)     |
              RSZ_CLK_EN(0)        |
              PRV_CLK_EN(0)        |
              HIST_CLK_EN(0)       |
              H3A_CLK_EN(0)        |
              CBUFF_AUTOGATING(0)  |
              CCDC_CLK_EN(1)       |
              SHIFT(0)             |
              PAR_CLK_POL(1)       |
              PAR_BRIDGE(0)        |
              PAR_SER_CLK_SEL(0)
              ,ISP_CTRL);
  data = omap_readl(ISP_CTRL);
  //printk("ISP_CTRL= 0x%x\n",data); 
}

//static void isp_SBL_config(void){
   ////printk("SBL_PCR             = 0x%x\n",omap_readl(SBL_PCR           ));
   ////printk("SBL_GLB_REG_0       = 0x%x\n",omap_readl(SBL_GLB_REG_0     ));
   ////printk("SBL_GLB_REG_1       = 0x%x\n",omap_readl(SBL_GLB_REG_1     ));
   ////printk("SBL_GLB_REG_2       = 0x%x\n",omap_readl(SBL_GLB_REG_2     ));
   ////printk("SBL_GLB_REG_3       = 0x%x\n",omap_readl(SBL_GLB_REG_3     ));
   ////printk("SBL_GLB_REG_4       = 0x%x\n",omap_readl(SBL_GLB_REG_4     ));
   ////printk("SBL_GLB_REG_5       = 0x%x\n",omap_readl(SBL_GLB_REG_5     ));
   ////printk("SBL_GLB_REG_6       = 0x%x\n",omap_readl(SBL_GLB_REG_6     ));
   ////printk("SBL_GLB_REG_7       = 0x%x\n",omap_readl(SBL_GLB_REG_7     ));
   ////printk("SBL_CCDC_WR_0       = 0x%x\n",omap_readl(SBL_CCDC_WR_0     ));
   ////printk("SBL_CCDC_WR_1       = 0x%x\n",omap_readl(SBL_CCDC_WR_1     ));
   ////printk("SBL_CCDC_WR_2       = 0x%x\n",omap_readl(SBL_CCDC_WR_2     ));
   ////printk("SBL_CCDC_WR_3       = 0x%x\n",omap_readl(SBL_CCDC_WR_3     ));
   ////printk("SBL_CCDC_FP_RD_0    = 0x%x\n",omap_readl(SBL_CCDC_FP_RD_0  ));
   ////printk("SBL_CCDC_FP_RD_1    = 0x%x\n",omap_readl(SBL_CCDC_FP_RD_1  ));
   ////printk("SBL_PRV_RD_0        = 0x%x\n",omap_readl(SBL_PRV_RD_0      ));
   ////printk("SBL_PRV_RD_1        = 0x%x\n",omap_readl(SBL_PRV_RD_1      ));
   ////printk("SBL_PRV_RD_2        = 0x%x\n",omap_readl(SBL_PRV_RD_2      ));
   ////printk("SBL_PRV_RD_3        = 0x%x\n",omap_readl(SBL_PRV_RD_3      ));
   ////printk("SBL_PRV_WR_0        = 0x%x\n",omap_readl(SBL_PRV_WR_0      ));
   ////printk("SBL_PRV_WR_1        = 0x%x\n",omap_readl(SBL_PRV_WR_1      ));
   ////printk("SBL_PRV_WR_2        = 0x%x\n",omap_readl(SBL_PRV_WR_2      ));
   ////printk("SBL_PRV_WR_3        = 0x%x\n",omap_readl(SBL_PRV_WR_3      ));
   ////printk("SBL_PRV_DK_RD_0     = 0x%x\n",omap_readl(SBL_PRV_DK_RD_0   ));
   ////printk("SBL_PRV_DK_RD_1     = 0x%x\n",omap_readl(SBL_PRV_DK_RD_1   ));
   ////printk("SBL_PRV_DK_RD_2     = 0x%x\n",omap_readl(SBL_PRV_DK_RD_2   ));
   ////printk("SBL_PRV_DK_RD_3     = 0x%x\n",omap_readl(SBL_PRV_DK_RD_3   ));
   ////printk("SBL_RSZ_RD_0        = 0x%x\n",omap_readl(SBL_RSZ_RD_0      ));
   ////printk("SBL_RSZ_RD_1        = 0x%x\n",omap_readl(SBL_RSZ_RD_1      ));
   ////printk("SBL_RSZ_RD_2        = 0x%x\n",omap_readl(SBL_RSZ_RD_2      ));
   ////printk("SBL_RSZ_RD_3        = 0x%x\n",omap_readl(SBL_RSZ_RD_3      ));
   ////printk("SBL_RSZ1_WR_0       = 0x%x\n",omap_readl(SBL_RSZ1_WR_0     ));
   ////printk("SBL_RSZ1_WR_1       = 0x%x\n",omap_readl(SBL_RSZ1_WR_1     ));
   ////printk("SBL_RSZ1_WR_2       = 0x%x\n",omap_readl(SBL_RSZ1_WR_2     ));
   ////printk("SBL_RSZ1_WR_3       = 0x%x\n",omap_readl(SBL_RSZ1_WR_3     ));
   ////printk("SBL_RSZ2_WR_0       = 0x%x\n",omap_readl(SBL_RSZ2_WR_0     ));
   ////printk("SBL_RSZ2_WR_1       = 0x%x\n",omap_readl(SBL_RSZ2_WR_1     ));
   ////printk("SBL_RSZ2_WR_2       = 0x%x\n",omap_readl(SBL_RSZ2_WR_2     ));
   ////printk("SBL_RSZ2_WR_3       = 0x%x\n",omap_readl(SBL_RSZ2_WR_3     ));
   ////printk("SBL_RSZ3_WR_0       = 0x%x\n",omap_readl(SBL_RSZ3_WR_0     ));
   ////printk("SBL_RSZ3_WR_1       = 0x%x\n",omap_readl(SBL_RSZ3_WR_1     ));
   ////printk("SBL_RSZ3_WR_2       = 0x%x\n",omap_readl(SBL_RSZ3_WR_2     ));
   ////printk("SBL_RSZ3_WR_3       = 0x%x\n",omap_readl(SBL_RSZ3_WR_3     ));
   ////printk("SBL_RSZ4_WR_0       = 0x%x\n",omap_readl(SBL_RSZ4_WR_0     ));
   ////printk("SBL_RSZ4_WR_1       = 0x%x\n",omap_readl(SBL_RSZ4_WR_1     ));
   ////printk("SBL_RSZ4_WR_2       = 0x%x\n",omap_readl(SBL_RSZ4_WR_2     ));
   ////printk("SBL_RSZ4_WR_3       = 0x%x\n",omap_readl(SBL_RSZ4_WR_3     ));
   ////printk("SBL_HIST_RD_0       = 0x%x\n",omap_readl(SBL_HIST_RD_0     ));
   ////printk("SBL_HIST_RD_1       = 0x%x\n",omap_readl(SBL_HIST_RD_1     ));
   ////printk("SBL_H3A_AF_WR_0     = 0x%x\n",omap_readl(SBL_H3A_AF_WR_0   ));
   ////printk("SBL_H3A_AF_WR_1     = 0x%x\n",omap_readl(SBL_H3A_AF_WR_1   ));
   ////printk("SBL_H3A_AEAWB_WR_0  = 0x%x\n",omap_readl(SBL_H3A_AEAWB_WR_0));
   ////printk("SBL_H3A_AEAWB_WR_1  = 0x%x\n",omap_readl(SBL_H3A_AEAWB_WR_1));
   ////printk("SBL_SDR_REQ_EXP     = 0x%x\n",omap_readl(SBL_SDR_REQ_EXP   ));
//}

static void isp_CCDC_config(void)
{
  //unsigned int data;
  //int k,n;
  //unsigned char * CptDataBuf;
  //unsigned char* CptDataBuf_phy;
 
  //printk("Before CptDataBuf =  kzalloc(512 * 512, GFP_KERNEL)\n");
  CptDataBuf =kzalloc(672 * 480, GFP_KERNEL); //  kzalloc(512 * 512, GFP_KERNEL);
  //CptDataBuf[10]=100;
  ////printk("CptData[10] = 0x%x\n", CptDataBuf[10]);
  //printk("Exit CptDataBuf =  kzalloc(512 * 512, GFP_KERNEL)\n");
 
  //printk("Before CptDataBuf_phy = (unsigned char *)virt_to_phys(CptDataBuf)\n");
  CptDataBuf_phy = (unsigned char *)virt_to_phys(CptDataBuf);
  //printk("Exit CptDataBuf_phy = (unsigned char *)virt_to_phys(CptDataBuf)\n");
  omap_writel(ENABLE(0), ISPCCDC_PCR);
      
  /* CCDC_SYN_MODE */       
  //omap_writel(0x00030723,ISPCCDC_SYN_MODE);
  omap_writel(SDR2RSZ(0) |
              VP2SDR(1)  |
              WEN(1)     |
              VDHDEN(1)  |
              //FLDSTAT  |
              LPF(0)     |
              INPMOD(0)  |
              PACK8(1)   |
              DATSIZ(7)  |
              FLDMODE(0) |
              DATAPOL(0) |
              EXWEN(0)   |   //外部写使能信号
              FLDPOL(0)  |
              HDPOL(0)   |
              VDPOL(0)   |
              FLDOUT(0)  |
              VDHDOUT(0)
              ,ISPCCDC_SYN_MODE);
 
    omap_writel(SPH(0) | NPN(671), ISPCCDC_HORZ_INFO);

  /* CCDC_VERT_START */                 
  omap_writel(SLV0(0) | SLV1(0), ISPCCDC_VERT_START); 
  
  /* CCDC_VERT_LINES */              
    omap_writel(NLV(479), ISPCCDC_VERT_LINES);
  /* CCDC_CULLING */                
  omap_writel(CULHEVN(0xff) |
              CULHODD(0xff) |
              CULV(0xff)
              ,ISPCCDC_CULLING);
               
  /* CCDC_HSIZE_OFF */                
    omap_writel(LNOFST(672), ISPCCDC_HSIZE_OFF );
 
  /* CCDC_SDOFST */
  omap_writel(FIINV(0)  |
              FOFST(0)  |
              LOFST0(0) |
              LOFST1(0) |
              LOFST2(0) |
              LOFST3(0)
              ,ISPCCDC_SDOFST ); 
             
  /* CCDC_SDR_ADDR */
 
  /* CCDC_CLAMP */  
  omap_writel(CLAMPEN(0) |
              OBSLEN(0)  |
              OBSLN(0)   |
              OBST(0)    |
              OBGAIN(0)
              ,ISPCCDC_CLAMP);
  
  /* CCDC_DCSUB */      
  omap_writel(DCSUB(0), ISPCCDC_DCSUB); 
 
 
  /* CCDC_BLKCMP */               
  omap_writel(R_YE(0)  |
              GR_CY(0) |
              GB_G(0)  |
              B_MG(0)
              ,ISPCCDC_BLKCMP);  
                
  /* CCDC_FPC */              
    
  /* CCDC_FPC_ADDR */            
  //omap_writel(  ADDR(a),ISPCCDC_FPC_ADDR  );
 
  omap_writel(FPERR(0) |
              FPCEN(0) |
              FPNUM(0)
              ,ISPCCDC_FPC);   
  
  /* CCDC_VDINT  */  
  omap_writel(VDINT0(0) |             
              VDINT1(0)
              ,ISPCCDC_VDINT);
  
  /* CCDC_ALAW */                
  omap_writel(CCDTBL(0) | GWDI(0), ISPCCDC_ALAW);           
               
  /****  CCDC_REC656IF */             
  omap_writel(ECCFVH(0) | R656ON(0), ISPCCDC_REC656IF);   
       
  /****  CCDC_CFG */            
  omap_writel(VDLC(1)    |
              MSBINVI(0) |
              BSWD(0)    |
              Y8POS(0)   |
              WENLOG(0)  |
              FIDMD(1)   |
              BW656(0)
              ,ISPCCDC_CFG);
      
  /****  CCDC_FMTCFG  */   
  omap_writel(VPIF_FRQ(0) |
              VPEN(0)     |
              VPIN(0)     |
              PLEN_EVEN(0)|
              PLEN_ODD(0) |
              LNUM(0)     |
              LNALT(0)    |
              FMTEN(0)   
              ,ISPCCDC_FMTCFG); 
               
 
           
  /* CCDC_LSC_CONFIG */              
  omap_writel(GAIN_MODE_M(0)       |    
              GAIN_MODE_N(0)       |    
              BUSY(0)              |    
              AFTER_REFORMATTER(0) |
              GAIN_FORMAT(0)       | 
              ENABLE(0)        
              ,ISPCCDC_LSC_CONFIG);
  

  //printk("Before omap_writel(CptDataBuf_phy, ISPCCDC_SDR_ADDR)\n");
  omap_writel((unsigned long)CptDataBuf_phy, ISPCCDC_SDR_ADDR);
  //printk("Exit omap_writel(CptDataBuf_phy, ISPCCDC_SDR_ADDR)\n");

  /* CCDC_PCR config */
  omap_writel(ENABLE(1), ISPCCDC_PCR);

 
 
 
 
 
//  while(1)
//  {
//      msleep(1000);      
//      omap_writel( (~ENABLE(1))& omap_readl(ISPCCDC_PCR) ,ISPCCDC_PCR);                                  
//      printk("Kernel_CptDataBuf[400]=%02X\n",CptDataBuf[400]);   
//      omap_writel( ENABLE(1),ISPCCDC_PCR);                                              
//  }
 
}

static void pin_mux(void)
{
  omap_writew((OFF_IN_PD  | IEN  | PTU | EN  | M0),ISP_CONTROL_PADCONF_CAM_HS);
  omap_writew((OFF_IN_PD  | IEN  | PTU | EN  | M0),ISP_CONTROL_PADCONF_CAM_VS);
  omap_writew((OFF_OUT_PD | IDIS | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_XCLKA);
  omap_writew((OFF_IN_PD  | IEN  | PTU | EN  | M0),ISP_CONTROL_PADCONF_CAM_PCLK);
  omap_writew((OFF_OUT_PD | IDIS | PTD | DIS | M4),ISP_CONTROL_PADCONF_CAM_FLD);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D0);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D1);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D2);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D3);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D4);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D5);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D6);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D7);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D8);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D9);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D10);
  omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_D11);
  //omap_writew((OFF_IN_PD  | IEN  | PTD | DIS | M4),ISP_CONTROL_PADCONF_CAM_WEN);
  omap_writew((OFF_OUT_PD | IDIS | PTD | DIS | M0),ISP_CONTROL_PADCONF_CAM_XCLKB);
}

static void isp_initconfig(void)
{
  //printk("Enter into isp_clk_config()\n");
  isp_clk_config();
  //printk("Exit isp_clk_config()\n");
 
  //printk("Enter into isp_pin_config()\n");
  isp_pin_config();
  //printk("Exit isp_pin_config()\n");
 
  //printk("Enter into pin_mux()\n");
  pin_mux();
  //printk("Exit pin_mux()\n");
 
  //printk("Enter into isp_timing_config()\n");
  isp_timing_config();
  //printk("Exit isp_timing_config()\n");
 
  //printk("Enter into isp_BridgeLane_config()\n");
  isp_BridgeLane_config();
  //printk("Exit isp_BridgeLane_config()\n");
 
  //printk("Enter into isp_CCDC_config()\n");
  isp_CCDC_config();
  //printk("Exit isp_CCDC_config()\n");
 
  //isp_SBL_config();
}

static int isp_open(struct inode *inode, struct file *file)
{
  int minor;

  minor = MINOR(inode->i_rdev);
  cam_isp_devices[minor]++;
 
  //printk(KERN_INFO "The camera isp device is opened!!!!!!\n");

  return 0;
}

static int isp_release(struct inode *inode, struct file *file)
{
  int minor;
 
  minor = MINOR(inode->i_rdev);
  if(cam_isp_devices[minor])
  {
    cam_isp_devices[minor]--;
  }
 
  //printk(KERN_INFO "The camera isp device is released!!!!!!\n");

  return 0;
}

static ssize_t isp_write(struct file *file, const char __user *buf, size_t count, loff_t *ppos)
{
  return 0;
}

static ssize_t isp_read(struct file *file, char __user *buf, size_t count, loff_t *ppos)
{
      unsigned long cnt;
      int aa;
     
      while(xieyuTag==0)  
      {   
          msleep(1);    
      }
          
      omap_writel( (~ENABLE(1))& omap_readl(ISPCCDC_PCR)  ,ISPCCDC_PCR);  //stop CCDC
     
      copy_to_user(buf, CptDataBuf, 512 * 512);                //If it is smaller than 512*512, it
                                                               //cannot be copied to user layer. Why?
                                                              
      printk("Kernel_CptDataBuf[400]=%02X\n",CptDataBuf[400]); //Only after running “copy_to_user” above,
                                                               // can  “Kernel_CptDataBuf[400]” be updated. Why?
                                                             

      xieyuTag=0;
     
      omap_writel( ENABLE(1),ISPCCDC_PCR);   //start CCDC
                      
     
      return count;
  
}

 

static int isp_ioctl(struct inode *inode, struct file *file, unsigned int command, unsigned long arg)
{
  return 0;
}

static struct file_operations isp_fops = {
 .owner  = THIS_MODULE,
 .read  = isp_read,
 .write  =   isp_write,
 .open  =   isp_open,
 .ioctl  =   isp_ioctl,
 .release = isp_release,
};


static irqreturn_t isp_irq(int irq, void *dev_id)
{
  if(omap_readl(ISP_IRQ0STATUS) & 0x80000000)
  {
    xieyuTag=1;
    omap_writel(0x80000000, ISP_IRQ0STATUS);
  }
  else
  {
    printk("No HS_VS_IRQ\n");
  }
//  printk("camera isp irq!\n");
  return 0;
}


static int __init isp_init(void)
{
  int result;
 
  result = register_chrdev(CAMERA_ISP_MAJOR, "ISP", &isp_fops);

  isp_initconfig();
 
    xieyuTag=0;

  int ret = request_irq(24, (irq_handler_t)isp_irq, IRQF_TRIGGER_RISING, "Camera ISP", NULL); 

  if(ret)
  {
    printk("Wow!!! ISP interrupt install failed! \n");
    return -1;
  }
  printk("request_irq() successfully registered!!!\n");

 

  return 0;
}

static void __exit isp_exit(void)
{
  free_irq(24,NULL);
  unregister_chrdev(CAMERA_ISP_MAJOR,"ISP");
}

module_init (isp_init);
module_exit (isp_exit);

MODULE_AUTHOR("xxx");
MODULE_DESCRIPTION("OMAP35xx Camera ISP driver");
MODULE_LICENSE("GPL");
//-----------------------------isp.c--end-----------------------------------------------


//=====================================================================================================
//=====================================Question========================================================
         Kernel Version:
                Linux version 2.6.31-rc7-omap1
        
         Question 1:
                In isp_read(), instead of running : copy_to_user(buf, CptDataBuf, 512 * 512),
                but run:  printk("Kernel_CptDataBuf[400]=%02X\n",CptDataBuf[400]);
                Then Kernel_CptDataBuf[400] will not be updated at all.
               
                In isp_read(), run:  copy_to_user(buf, CptDataBuf, 512 * 512);
                Then run: printk("Kernel_CptDataBuf[400]=%02X\n",CptDataBuf[400]);
                Then Kernel_CptDataBuf[400] will be updated basically, but usually only after it is
                recalled 2~3 times, can isp_read() CptDataBuf[400] be updated once. That is to say,
                the data is updated, but not in real time.
               
         Question 2: Take the code isp.c in the case above for example, make changes like this:
                In isp_init(), delete request_irq();
                In isp_exit(), delete free_irq(24,NULL);
                At the end of the function isp_CCDC_config(), add                                   
                      while(1)
                      {
                          msleep(1000);      
                          omap_writel( (~ENABLE(1))& omap_readl(ISPCCDC_PCR) ,ISPCCDC_PCR);                                  
                          printk("Kernel_CptDataBuf[400]=%02X\n",CptDataBuf[400]);   
                          omap_writel( ENABLE(1),ISPCCDC_PCR);                                              
                      }
                Run the command "busybox-omap insmod  ./isp.ko"
                Result: The printed Kernel_CptDataBuf[400] is not updated, but updated once after
                        waiting for over 10 minutes occasionally.
                       
               
                Remove the infinite loop from the codes above, and change to:           
                //while(1)
                //{
                    msleep(1000);      
                    omap_writel( (~ENABLE(1))& omap_readl(ISPCCDC_PCR) ,ISPCCDC_PCR);                                  
                    printk("Kernel_CptDataBuf[400]=%02X\n",CptDataBuf[400]);   
                    omap_writel( ENABLE(1),ISPCCDC_PCR);                                              
                //}
               
               run it continuously
                while(1)
                {
                    system("busybox-omap rmmod  isp.ko");
                    system("busybox-omap insmod  ./isp.ko");
                }
                Result: the printed Kernel_CptDataBuf[400] is updated every time.

  •            I have set the "ISPCCDC_SDR_ADDR"  and  ENABLE the "ISPCCDC_PCR",and 
               the corresponding memory must updata when the ISP interface's datas updata by the
               FPGA automatically.I think the memory which the "ISPCCDC_SDR_ADDR"  define updata should not relation to
               the "copy_to_user", but actually, I find it is not.Is there problem in my test problem? Could you help me
                to find? Thanks a lot.

  • In the code above, I just read a single frame was not a problem. the problem is that when I loop to read, it always Always drop frames, Sometimes drop one frames and sometimes drop 2 frames,the wost case drop 9 frames.IS there some problem in my code when I loop to read? Thanks!

  • This was a hardware issue, the timing from the external camera did not meet the min hsync blank time requirements. This is now resolved.

    Regards,
    Punya