This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question regarding DMA usage with DM355 + MPEG4 encoder



Hi,

We are using the DM355 + DVEVM 2.0 + CE 2.23 + MPEG4 Simple Profile Encoder 1.13.000.

I am reading the encoder datasheet, SPRS488e.pdf, with a short abstract about DDR Bandwidth Usage.

 

Would be possible to get more detailed information about codec DMA usage? Like DMA channels used, data transferred through DMA, etc.

 

Thank you very much.

 

Kind Regards.

Gerardo

 

  • Hi,

     

    The DMA channels used are mentioned in the 'Features' section of the Datasheet. 

    As for data transferred through DMA -- can you be a bit more specific as to what information you are looking for and in what context? Then I can get back to you accordingly.

     

    Regards,

    Akshay