Part Number: TDA2SX
Dear TI,
I am working with my custom board. I can now bring up the board successfully.
But the kernel may not startup aumatically.
This problem may occure after the some files be modified in the boot or rootfs partitions.
I am not quite sure what's the root cause.
Every time i encounter this problem, i need issue "boot" command in the u-boot cli. Then the kernel could be booted normally.
The attached file is the entire startup log file. Hope reply!
Regards,
Liu Gan
U-Boot SPL 2016.05-svn1450 (Sep 23 2019 - 21:43:33)
DRA752-GP ES2.0
Trying to boot from MMC2_2
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
no pinctrl for hs
[LG_mmc_startup_1873]: eMMC.
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
Jumping to U-Boot
loaded - jumping to U-Boot...
U-Boot 2016.05-svn1450 (Sep 23 2019 - 21:43:33 +0800)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: HiRain DRA74x Board REV H.0
DRAM: 2 GiB
Relocation Offset is: 7e744000
Relocating to fef44000, new gd at fdf23eb8, sp at fdf0fcf0
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
[LG_mmc_startup_1873]: eMMC.
*** Warning - bad CRC, using default environment
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: No ethernet found.
Hit any key to stop autoboot: 0
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
failed to set signal voltage
Card did not respond to voltage select!
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
failed to set signal voltage
Card did not respond to voltage select!
i2c_write: error waiting for data ACK (status=0x116)
tps65903x: could not set LDO1 voltage.
failed to set signal voltage
Card did not respond to voltage select!
[LG_mmc_startup_1873]: eMMC.
switch to partitions #0, OK
mmc1(part 0) is current device
[LG_mmc_startup_1873]: eMMC.
mmc - MMC sub system
Usage:
mmc info - display info of the current MMC device
mmc read addr blk# cnt
mmc write addr blk# cnt
mmc erase blk# cnt
mmc rescan
mmc part - lists available partition on current mmc device
mmc dev [dev] [part] - show or set current mmc device [partition]
mmc list - lists available devices
mmc hwpartition [args...] - does hardware partitioning
arguments (sizes in 512-byte blocks):
[user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
[gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
[check|set|complete] - mode, complete set partitioning completed
WARNING: Partitioning is a write-once setting once it is set to complete.
Power cycling is required to initialize partitions after set to complete.
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev boot_ack boot_partition partition_access
- Change the bits of the PARTITION_CONFIG field of the specified device
mmc rst-function dev value
- Change the RST_n_FUNCTION field of the specified device
WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
mmc setdsr <value> - set DSR register value
mmc - MMC sub system
Usage:
mmc info - display info of the current MMC device
mmc read addr blk# cnt
mmc write addr blk# cnt
mmc erase blk# cnt
mmc rescan
mmc part - lists available partition on current mmc device
mmc dev [dev] [part] - show or set current mmc device [partition]
mmc list - lists available devices
mmc hwpartition [args...] - does hardware partitioning
arguments (sizes in 512-byte blocks):
[user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
[gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
[check|set|complete] - mode, complete set partitioning completed
WARNING: Partitioning is a write-once setting once it is set to complete.
Power cycling is required to initialize partitions after set to complete.
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev boot_ack boot_partition partition_access
- Change the bits of the PARTITION_CONFIG field of the specified device
mmc rst-function dev value
- Change the RST_n_FUNCTION field of the specified device
WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
mmc setdsr <value> - set DSR register value
Booting from eMMC ...
Wrong Image Format for bootm command
ERROR: can't get kernel image!
=> mmc info
Device: OMAP SD/MMC
Manufacturer ID: 11
OEM: 100
Name: 008G3
Tran Speed: 52000000
Rd Block Len: 512
MMC version 4.0
High Capacity: Yes
Capacity: 7.3 GiB
Bus Width: 8-bit DDR
Erase Group Size: 512 KiB
=> printenv
arch=arm
args_fit=setenv bootargs console=${console}
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=tda2xx
board_findfdt=if test $board_name = hirain-tda2xx; then setenv fdtfile hirain-tda2xx.dtb; fi;
board_name=hirain-tda2xx
board_rev=H.0
boot_fdt=try
boot_fit=0
boot_os=0
boot_part=9
bootargs=androidboot.serialno=1500c007650608a2
bootcmd=if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; saveenv;echo Booting into fastboot ...; fastboot 0; fi;if test ${boot_fit} -eq 1; then run update_to_fit;fi;run findfdt; run envboot; run mmcboot;run emmc_android_boot;
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=zImage
bootm_size=0x10000000
bootpart=1:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO0,115200n8
cpu=armv7
dfu_alt_info_emmc=rawemmc raw 0 3751936;boot part 1 1;rootfs part 1 2;MLO fat 1 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 1 1;spl-os-image fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 0 1;spl-os-image fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1
dfu_alt_info_qspi=MLO raw 0x0 0x040000;u-boot.img raw 0x040000 0x0100000;u-boot-spl-os raw 0x140000 0x080000;u-boot-env raw 0x1C0000 0x010000;u-boot-env.backup raw 0x1D0000 0x010000;kernel raw 0x1E0000 0x800000
dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
dfu_bufsiz=0x10000
dofastboot=0
emmc_android_boot=setenv eval_bootargs setenv bootargs $bootargs; run eval_bootargs; setenv mmcdev 1; setenv fdt_part 3; setenv boot_part 9; if test $reboot_image = recovery; then setenv boot_part 8; setenv reboot_image boot; saveenv; fi;setenv machid fe6; mmc dev $mmcdev; mmc rescan; part start mmc ${mmcdev} ${fdt_part} fdt_start; part size mmc ${mmcdev} ${fdt_part} fdt_size; part start mmc ${mmcdev} ${boot_part} boot_start; part size mmc ${mmcdev} ${boot_part} boot_size; mmc read ${fdtaddr} ${fdt_start} ${fdt_size}; mmc read ${loadaddr} ${boot_start} ${boot_size}; echo Booting from eMMC ...; bootm $loadaddr $loadaddr $fdtaddr;
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
eval_bootargs=setenv bootargs androidboot.serialno=${serial#}
fdt_addr_r=0x88000000
fdt_part=3
fdtaddr=0x88000000
fdtcontroladdr=fdf0fd18
fdtfile=hirain-tda2xx.dtb
findfdt=if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.dtb; fi; if test $board_name = dra7xx; then setenv fdtfile dra7-evm.dtb; fi;if test $board_name = dra72x-revc; then setenv fdtfile dra72-evm-revc.dtb; fi;if test $board_name = dra72x; then setenv fdtfile dra72-evm.dtb; fi;if test $board_name = dra71x; then setenv fdtfile dra71-evm.dtb; fi;if test $board_name = dra76x; then setenv fdtfile dra76-evm.dtb; fi;if test $board_name = beagle_x15; then setenv fdtfile am57xx-beagle-x15.dtb; fi;if test $board_name = beagle_x15_revb1; then setenv fdtfile am57xx-beagle-x15-revb1.dtb; fi;if test $board_name = am57xx_evm; then setenv fdtfile am57xx-evm.dtb; fi;if test $board_name = am57xx_evm_reva3; then setenv fdtfile am57xx-evm-reva3.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = no; then setenv fdtfile am572x-idk.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am572x-idk-lcd-osd.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am572x-idk-lcd-osd101t2587.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = no; then setenv fdtfile am571x-idk.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am571x-idk-lcd-osd.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am571x-idk-lcd-osd101t2587.dtb; fi;if test $board_findfdt != undefined; then run board_findfdt; fi;if test $fdtfile = undefined; then echo WARNING: Could not determine device tree to use; fi;
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage.itb
fit_loadaddr=0x88000000
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=fatload mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_fit; bootm ${loadaddr}#${fdtfile};
loadimage=load mmc ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
machid=fe6
mmcboot=if mmc dev ${mmcdev}; then setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then run loadfdt; echo Booting from mmc${mmcdev} ...; run args_mmc; bootz ${loadaddr} - ${fdtaddr}; fi; fi; fi;
mmcdev=1
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
nfsopts=nolock
partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
partitions_android=uuid_disk=${uuid_gpt_disk};name=xloader,start=128K,size=256K,uuid=${uuid_gpt_xloader};name=bootloader,size=2304K,uuid=${uuid_gpt_bootloader};name=environment,size=256K,uuid=${uuid_gpt_environment};name=misc,size=128K,uuid=${uuid_gpt_misc};name=reserved,size=384K,uuid=${uuid_gpt_reserved};name=efs,size=16M,uuid=${uuid_gpt_efs};name=crypto,size=16K,uuid=${uuid_gpt_crypto};name=recovery,size=30M,uuid=${uuid_gpt_recovery};name=boot,size=10M,uuid=${uuid_gpt_boot};name=system,size=768M,uuid=${uuid_gpt_system};name=vendor,size=256M,uuid=${uuid_gpt_vendor};name=cache,size=256M,uuid=${uuid_gpt_cache};name=ipu1,size=8M,uuid=${uuid_gpt_ipu1};name=ipu2,size=8M,uuid=${uuid_gpt_ipu2};name=dsp1,size=8M,uuid=${uuid_gpt_dsp1};name=dsp2,size=8M,uuid=${uuid_gpt_dsp2};name=userdata,size=-,uuid=${uuid_gpt_userdata}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rdaddr=0x88080000
reboot_image=boot
rootpath=/export/rootfs
scriptaddr=0x80000000
scsidevs=0
serial#=1500c007650608a2
soc=omap5
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@4806a000
stdin=serial@4806a000
stdout=serial@4806a000
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usbtty=cdc_acm
vendor=hirain
ver=U-Boot 2016.05-svn1450 (Sep 23 2019 - 21:43:33 +0800)
vram=16M
Environment size: 7542/131067 bytes
=> boot
[LG_mmc_startup_1873]: eMMC.
switch to partitions #0, OK
mmc1(part 0) is current device
[LG_mmc_startup_1873]: eMMC.
SD/MMC found on device 1
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
217 bytes read in 2 ms (105.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
[LG_mmc_startup_1873]: eMMC.
switch to partitions #0, OK
mmc1(part 0) is current device
[LG_mmc_startup_1873]: eMMC.
SD/MMC found on device 1
3560560 bytes read in 56 ms (60.6 MiB/s)
107263 bytes read in 6 ms (17 MiB/s)
Booting from mmc1 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x365470 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe2000, end 8ffff2fe ... OK
Using machid 0xfe6 from environment
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84-svn1450 (gan.liu@ubuntu) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #6 SMP PREEMPT Mon Sep 23 21:09:24 CST 2019
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000fd400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000fed00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @eed49000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 509504
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=4590e133-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1417252K/2044928K available (6635K kernel code, 320K rwdata, 2392K rodata, 336K init, 290K bss, 422876K reserved, 204800K cma-reserved, 1266688K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08d902c (9029 kB)
[ 0.000000] .init : 0xc08da000 - 0xc092e000 ( 336 kB)
[ 0.000000] .data : 0xc092e000 - 0xc097e120 ( 321 kB)
[ 0.000000] .bss : 0xc0980000 - 0xc09c8800 ( 290 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000016] Switching to timer-based delay loop, resolution 162ns
[ 0.000337] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000345] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000790] Console: colour dummy device 80x30
[ 0.000805] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000812] This ensures that you still see kernel messages. Please
[ 0.000817] update your kernel commandline.
[ 0.000831] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000844] pid_max: default: 32768 minimum: 301
[ 0.000942] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000952] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001492] Initializing cgroup subsys io
[ 0.001509] Initializing cgroup subsys memory
[ 0.001533] Initializing cgroup subsys devices
[ 0.001545] Initializing cgroup subsys freezer
[ 0.001557] Initializing cgroup subsys perf_event
[ 0.001568] Initializing cgroup subsys pids
[ 0.001595] CPU: Testing write buffer coherency: ok
[ 0.001796] /cpus/cpu@0 missing clock-frequency property
[ 0.001813] /cpus/cpu@1 missing clock-frequency property
[ 0.001823] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001861] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.080069] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080137] Brought up 2 CPUs
[ 0.080150] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080157] CPU: All CPU(s) started in HYP mode.
[ 0.080162] CPU: Virtualization extensions available.
[ 0.080542] devtmpfs: initialized
[ 0.109149] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.110115] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.313382] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.313406] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.317853] pinctrl core: initialized pinctrl subsystem
[ 0.318726] NET: Registered protocol family 16
[ 0.319636] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350237] cpuidle: using governor ladder
[ 0.380262] cpuidle: using governor menu
[ 0.388802] OMAP GPIO hardware version 0.1
[ 0.395290] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.411292] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.411305] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.418760] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.418771] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.419233] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.419243] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.419818] OMAP DMA hardware revision 0.0
[ 0.461512] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.462640] edma 43300000.edma: memcpy is disabled
[ 0.467417] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.471737] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.471918] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.472075] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.472237] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.472520] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.472708] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.475707] palmas 2-0058: IRQ missing: skipping irq request
[ 0.491143] palmas: probe of 2-0058 failed with error -121
[ 0.491170] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.491357] media: Linux media interface: v0.10
[ 0.491408] Linux video capture interface: v2.00
[ 0.491446] pps_core: LinuxPPS API ver. 1 registered
[ 0.491453] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.491476] PTP clock support registered
[ 0.491519] EDAC MC: Ver: 3.0.0
[ 0.492295] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.492593] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.492936] Advanced Linux Sound Architecture Driver Initialized.
[ 0.493764] clocksource: Switched to clocksource arch_sys_counter
[ 0.504107] NET: Registered protocol family 2
[ 0.504593] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.504657] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.504782] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.504829] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.504860] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.505063] NET: Registered protocol family 1
[ 0.505319] RPC: Registered named UNIX socket transport module.
[ 0.505329] RPC: Registered udp transport module.
[ 0.505336] RPC: Registered tcp transport module.
[ 0.505343] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.506289] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.516395] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.517054] NFS: Registering the id_resolver key type
[ 0.517086] Key type id_resolver registered
[ 0.517094] Key type id_legacy registered
[ 0.517163] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.518455] bounce: pool size: 64 pages
[ 0.518605] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.518622] io scheduler noop registered
[ 0.518637] io scheduler deadline registered
[ 0.518673] io scheduler cfq registered (default)
[ 0.523053] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.526262] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.526274] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.526306] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.526327] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.556119] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.556294] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.556306] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.556317] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.556326] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.556726] PCI: bus0: Fast back to back transfers disabled
[ 0.556848] PCI: bus1: Fast back to back transfers enabled
[ 0.556931] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.556946] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.556958] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.557175] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.617731] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.621088] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.616399] console [ttyS0] enabled
[ 1.620790] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.630489] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.640479] [drm] Initialized drm 1.1.0 20060810
[ 1.646017] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.652662] [drm] No driver support for vblank timestamp query.
[ 1.658833] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
[ 1.671713] loop: module loaded
[ 1.675225] vmemexp device MAJOR num = 245
[ 1.679356] vmemexp class registered
[ 1.683070] /dev/vmemexp device registered
[ 1.687205] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 1.692893] nand: No NAND device found
[ 1.696684] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 1.706457] m25p80 spi32766.0: unrecognized JEDEC id bytes: 00, 0, 0
[ 1.714030] libphy: Fixed MDIO Bus: probed
[ 1.763800] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.769924] davinci_mdio 48485000.mdio: no live phy, scanning all
[ 1.873765] davinci_mdio 48485000.mdio: timed out waiting for user access
[ 1.973764] davinci_mdio 48485000.mdio: timed out waiting for idle
[ 1.979994] davinci_mdio: probe of 48485000.mdio failed with error -5
[ 1.987115] cpsw 48484000.ethernet: Detected MACID = a8:e2:c1:08:a5:34
[ 1.993782] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 2.000750] cpsw 48484000.ethernet: cpsw: Detected MACID = a8:e2:c1:08:a5:35
[ 2.009359] mousedev: PS/2 mouse device common for all mice
[ 2.015567] i2c /dev entries driver
[ 2.024071] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.029695] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.036154] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.117075] mmc0: MAN_BKOPS_EN bit is not set
[ 2.125895] mmc0: mmc_select_hs200 failed, error -74
[ 2.130882] : switch to mmc0 failed
[ 2.135540] mmc0: new MMC card at address 0001
[ 2.150477] mmcblk0: mmc0:0001 008G30 7.28 GiB
[ 2.165327] mmcblk0boot0: mmc0:0001 008G30 partition 1 8.00 MiB
[ 2.171505] mmcblk0boot1: mmc0:0001 008G30 partition 2 8.00 MiB
[ 2.179214] mmcblk0: p1 p2
[ 2.194588] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.206970] NET: Registered protocol family 10
[ 2.212263] sit: IPv6 over IPv4 tunneling driver
[ 2.217578] NET: Registered protocol family 17
[ 2.222304] Key type dns_resolver registered
[ 2.226762] omap_voltage_late_init: Voltage driver support not added
[ 2.233788] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.240056] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.247381] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 2.253993] Power Management for TI OMAP4+ devices.
[ 2.259106] Registering SWP/SWPB emulation handler
[ 2.265267] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.272841] dmm 4e000000.dmm: initialized all PAT entries
[ 2.279340] [drm] Initialized omapdrm 1.0.0 20110917 on minor 1
[ 2.286986] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.292451] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.298730] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.304990] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 2.311995] hctosys: unable to open rtc device (rtc0)
[ 2.329003] evm_1v8: disabling
[ 2.332081] aic_dvdd: disabling
[ 2.335261] vmmcwl_fixed: disabling
[ 2.338771] pbias_mmc_omap5: disabling
[ 2.342748] ALSA device list:
[ 2.345740] No soundcards found.
[ 2.378797] EXT4-fs (mmcblk0p2): recovery complete
[ 2.384659] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.392813] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.406709] devtmpfs: mounted
[ 2.409908] Freeing unused kernel memory: 336K
[ 2.414390] This architecture does not have kernel memory protection.
[ 2.618201] systemd[1]: System time before build time, advancing clock.
[ 2.658352] random: systemd: uninitialized urandom read (16 bytes read, 7 bits of entropy available)
[ 2.671077] random: systemd: uninitialized urandom read (16 bytes read, 7 bits of entropy available)
[ 2.682677] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 2.701195] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 2.725195] systemd[1]: Set hostname to <dra7xx-evm>.
[ 2.803337] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 8 bits of entropy available)
[ 2.813998] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 8 bits of entropy available)
[ 2.815881] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 8 bits of entropy available)
[ 2.841561] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 9 bits of entropy available)
[ 2.859638] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 10 bits of entropy available)
[ 2.907184] random: systemd: uninitialized urandom read (16 bytes read, 12 bits of entropy available)
[ 2.916861] random: systemd: uninitialized urandom read (16 bytes read, 12 bits of entropy available)
[ 2.926822] random: systemd: uninitialized urandom read (16 bytes read, 12 bits of entropy available)
[ 3.195147] systemd[1]: basic.target: Found ordering cycle on basic.target/start
[ 3.202591] systemd[1]: basic.target: Found dependency on sockets.target/start
[ 3.209967] systemd[1]: basic.target: Found dependency on dbus.socket/start
[ 3.217004] systemd[1]: basic.target: Found dependency on sysinit.target/start
[ 3.224305] systemd[1]: basic.target: Found dependency on alignment.service/start
[ 3.231828] systemd[1]: basic.target: Found dependency on basic.target/start
[ 3.238931] systemd[1]: basic.target: Breaking ordering cycle by deleting job sockets.target/start
[ 3.247948] systemd[1]: sockets.target: Job sockets.target/start deleted to break ordering cycle starting with basic.target/start
[ SKIP ] Ordering cycle found, skipping Sockets
[ 3.284150] systemd[1]: alignment.service: Found ordering cycle on alignment.service/start
[ 3.292461] systemd[1]: alignment.service: Found dependency on sysinit.target/start
[ 3.300211] systemd[1]: alignment.service: Found dependency on alignment.service/start
[ 3.308217] systemd[1]: alignment.service: Breaking ordering cycle by deleting job alignment.service/start
[ 3.317959] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with alignment.service/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 3.356140] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 3.384221] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 3.414031] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.444089] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 3.473966] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.505425] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 3.534674] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 3.574334] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.604732] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 3.634630] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.664203] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 3.694091] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 3.714098] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 3.744094] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 3.814265] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 3.834649] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 3.869237] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 3.897529] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 3.926540] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 3.956686] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 3.973960] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 3.986779] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 4.014110] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 4.034147] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.094267] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.124085] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 4.189182] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 4.214192] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 4.244067] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 4.264262] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Setup Virtual Console.
Starting udev Coldplug all Devices...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 5.039342] systemd-journald[138]: Received request to flush runtime journal from PID 1
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started udev Coldplug all Devices.
[ 5.492709] omap-rproc 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
[ 5.513005] remoteproc0: 58820000.ipu is available
[ 5.521008] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 5.532791] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 5.551089] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 5.555861] remoteproc0: Direct firmware load for dra7-ipu1-fw.xem4 failed with error -2
[ 5.565923] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 5.593443] remoteproc0: failed to load dra7-ipu1-fw.xem4
[ 5.615665] Adding alas for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 5.621807] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 5.628126] remoteproc1: 55020000.ipu is available
[ 5.633031] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 5.644596] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
Starting Load/Save Random Seed...[ 5.657287] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 5.684958] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 5.696644] omap-rproc 40800000.dsp: assigned eserved memory node dsp1_cma@99000000
[ OK ] Reached target Local File Systems.[ 5.710851] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 5.725920] remoteproc2: 40800000.dsp is available
[ 5.730828] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 5.747553] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 5.762424] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 5.771435] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guarnteed.
Starting Create Volatile Files and Directories...
[ 5.820275] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[ 5.821815] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 5.844219] remoteproc3: 41000000.dsp is available
[ 5.844946] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 5.844951] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 5.844988] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 5.895354] remoteproc3: Note: remoteproc is still under development and considered experimental.
[ 5.905229] remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ OK ] Started Load/Save Random Seed.[ 5.931447] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ OK ] Started Create Volatile Files and Directories.
[ 5.980099] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 6.018287] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ OK ] Found device /dev/ttyS0.
[ 6.035164] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ 6.448112] remoteproc2: registered virtio0 (type 7)
[ 6.464973] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 6.473586] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 6.480227] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 6.486502] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 6.493415] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 6.534152] SCSI subsystem initialized
[ 6.700884] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 6.724805] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 6.729726] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 6.759555] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 6.774976] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 6.783560] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 6.787591] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 6.787660] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 6.790695] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 6.808116] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ 6.823260] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 6.840781] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ OK ] Started Network Time Synchronization.
[ 6.862985] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 6.883694] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 6.896142] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 6.904400] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
Starting Synchronize System and HW clocks...
[ 6.975130] remoteproc1: registered virtio1 (type 7)
[ OK ] Reached target System Time Synchronized.
[ 7.048310] CAN device driver interface
[ 7.205732] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=352)
[ 7.226561] omap_hsmmc 4809c000.mmc: Got CD GPIO
[FAILED] Failed to start Synchronize System and HW clocks.[ 7.238343] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 7.252066] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 7.258536] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
See 'systemctl status sync-clocks.service' for details.
[ OK ] Reached target System Initialization.
[ OK ] Reached target Basic System.
[ 7.612668] remoteproc3: registered virtio2 (type 7)
[ 7.665747] [drm] Initialized pvr 1.14.3699939 20110701 on minor 2
[ 7.677295] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 7.680773] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 7.692106] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ OK ] Started System Logging Service.
[ 7.714876] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 7.721274] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 7.721279] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 7.721320] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
Starting rc.pvr.service...
[ 7.825261] scsi host0: ahci
[ 7.828698] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 341
[ 7.859172] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on D-Bus System Message Bus Socket.[ 7.895935] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 7.939663] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ 7.943406] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 7.943511] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ OK ] Started D-Bus System Message Bus.
Starting Network Service...
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ 8.193509] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 8.204700] ata1: SATA link down (SStatus 0 SControl 300)
[ OK ] Started Kernel Logging Service.
[ 8.241638] net eth1: initializing cpsw version 1.15 (0)
[ 8.258317] net eth0: initialized cpsw ale version 1.4
Starting Permit User Sessions...
[ 8.277428] net eth0: ALE Table size 1024
[ 8.293144] libphy: PHY 48485000.mdio:03 not found
Starting Login Service...
[ 8.318351] net eth1: phy "48485000.mdio:03" not found on slave 1, err -19
[ 8.356736] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 8.365102] remoteproc2: powering up 40800000.dsp
[ 8.396482] remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 6986764
[ 8.403624] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
[ 8.403663] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 8.403718] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 8.408885] net eth0: initializing cpsw version 1.15 (0)
[ 8.411885] libphy: PHY 48485000.mdio:02 not found
[ 8.411895] net eth0: phy "48485000.mdio:02" not found on slave 0, err -19
[ 8.431715] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 8.496445] remoteproc2: remote processor 40800000.dsp is now up
[ 8.519165] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 8.520267] remoteproc1: powering up 55020000.ipu
[ 8.522165] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 8.529195] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 8.529200] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 8.529248] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 8.555623] remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 10183852
[ 8.555719] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 8.617652] remoteproc1: remote processor 55020000.ipu is now up
[ 8.619431] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 8.620507] remoteproc3: powering up 41000000.dsp
[ 8.622706] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 8.634578] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 8.634583] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 8.634619] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 8.641769] remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 6986764
[ 8.648814] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[ 8.648851] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[ 8.648961] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[ OK ] Started Network Service.
[ 8.705597] remoteproc3: remote processor 41000000.dsp is now up
[ 8.717217] virtio_rpmsg_bus virtio2: rpmsg host is online
[ OK ] Started rc.pvr.service.[ 8.726132] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 8.736958] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 8.743347] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ OK ] Started Permit User Sessions.
[ 8.768370] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 8.871137] virtio_rpmsg_bus virtio1: creating channel rpmsg-proto addr 0x50
[ 8.893965] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x50
[ 8.901196] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x50
[ 8.931053] NET: Registered protocol family 41
[ 8.940894] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 8.956282] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 8.962502] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 8.970759] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517