Part Number: AM5728
Tool/software: Code Composer Studio
Hello,
I have some troubles to get interrupts from input capture ECAP1. Below is part of the code I wrote:
1. Pinmux setting acording to my HW into the library:
void PinmuxECAP1Config()
{
Uint32 regVal = 0U;
regVal = 0U;
CSL_FINST(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_WAKEUPENABLE, DISABLE);
CSL_FINST(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_INPUTENABLE, ENABLE);
CSL_FINST(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_PULLTYPESELECT, PULL_UP);
CSL_FINST(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_PULLUDENABLE, ENABLE);
CSL_FINST(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_MODESELECT, MUX_MODE);
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_DELAYMODE, 0U);
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_VIN2A_D2_VIN2A_D2_MUXMODE, 10U);
((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_VIN2A_D2 = regVal;
}
2. activate the clock of the PWMSS1 module into the library:
CSL_FINST(l4PerCmReg->CM_L4PER2_PRUSS1_CLKCTRL_REG,
L4PER_CM_CORE_COMPONENT_CM_L4PER2_PRUSS1_CLKCTRL_REG_MODULEMODE, ENABLE);
while(CSL_L4PER_CM_CORE_COMPONENT_CM_L4PER2_PWMSS1_CLKCTRL_REG_IDLEST_FUNC !=
CSL_FEXT(l4PerCmReg->CM_L4PER2_PRUSS1_CLKCTRL_REG,
L4PER_CM_CORE_COMPONENT_CM_L4PER2_PRUSS1_CLKCTRL_REG_IDLEST));
3. ECAP1 interrupt setting in the application:
/* XBar configuration */
CSL_xbarIrqConfigure (CSL_XBAR_IRQ_CPU_ID_DSP1, CSL_XBAR_INST_DSP1_IRQ_32, CSL_XBAR_PWMSS1_IRQ_eCAP0INT);
Intc_Init();
Intc_IntEnable(0);
/* Register ISR */
Intc_IntRegister(APP_ECAP1_INT, (IntrFuncPtr) AppEcapIntrISR, 0);
Intc_IntPrioritySet(APP_ECAP1_INT, 1, 0);
Intc_SystemEnable(APP_ECAP1_INT);
4. ECAP1 module initialisation:
/* enables clock for ECAP module */
ECAPClockEnable(ECAP_BASE_ADDRESS);
/* Disable all capture interrupts */
ECAPIntDisable(ECAP_BASE_ADDRESS, ECAP_ECEINT_CEVT1 |
ECAP_ECEINT_CEVT2 |
ECAP_ECEINT_CEVT3 |
ECAP_ECEINT_CEVT4 |
ECAP_ECEINT_CTROVF |
ECAP_ECEINT_CTR_PRD |
ECAP_ECEINT_CTR_CMP);
/* Clear all CAP interrupt flags */
ECAPGlobalIntEnable(ECAP_BASE_ADDRESS);
/* Disable CAP1-4 register loads at capture event time */
ECAPCaptureLoadingDisable(ECAP_BASE_ADDRESS);
/* Stop the counter */
ECAPCounterControl(ECAP_BASE_ADDRESS, ECAP_COUNTER_STOP);
/* Capture Events on Rising Edge */
ECAPCapeEvtPolarityConfig(ECAP_BASE_ADDRESS, ECAP_CAPPOL_RE, // Capture Event 1 polarity
ECAP_CAPPOL_RE, // Capture Event 2 polarity
ECAP_CAPPOL_RE, // Capture Event 3 polarity
ECAP_CAPPOL_RE); // Capture Event 4 polarity
/* Do not reset counter on Capture Event (absolute time stamp) */
ECAPCaptureEvtCntrRstConfig(ECAP_BASE_ADDRESS, ECAP_CTRRST_ABS_MODE, // Counter reset on Capture Event 1
ECAP_CTRRST_ABS_MODE, // Counter reset on Capture Event 2
ECAP_CTRRST_ABS_MODE, // Counter reset on Capture Event 3
ECAP_CTRRST_ABS_MODE); // Counter reset on Capture Event 4
/* Enable CAP1-4 register loads at capture event time */
ECAPCaptureLoadingEnable(ECAP_BASE_ADDRESS);
/* By-pass the prescaler */
ECAPPrescaleConfig(ECAP_BASE_ADDRESS, ECAP_PRESCALE_DIV1);
/* ECAP module operates in capture mode */
ECAPOperatingModeSelect(ECAP_BASE_ADDRESS, ECAP_CAPTURE_MODE);
/* Operate in continuous mode */
ECAPContinousModeConfig(ECAP_BASE_ADDRESS);
/* Disable sync-in option & sync-out signal */
ECAPSyncInOutSelect(ECAP_BASE_ADDRESS, ECAP_SYNC_IN_DISABLE, ECAP_SYNC_OUT_DISABLE);
/* TSCTR free-running */
ECAPCounterControl(ECAP_BASE_ADDRESS, ECAP_COUNTER_FREE_RUNNING);
/* Interrupt on Event 1 */
ECAPIntEnable(ECAP_BASE_ADDRESS, ECAP_ECEINT_CEVT1);
The input is toggling with a TTL square signal but the ISR sub-routine never trigs... Do you have any suggestion to help to figure out the issue?
Thanks in advance,
Sylvain