Dear Sir,
I'm using DM355EVM and dvsdk_1_30_00_40.
I can't use /dev/fb/0 (OSD plane) if the EVM boot from NAND flash.
I can use it using NFS root filesystem.
The related bootargs option is below.
>video=dm355fb:vid0=640x480x16,2500K:vid1=640x480x16,2500K:osd0=640x480x16,2400K
I tried copying NFS's /etc to NAND's /etc.
Then, I can use OSD even if booting from NAND flash.
Where of /etc is the difference?
Best regards,
Yoshiki Komatsudaira.