This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5746: Processor recommendation

Part Number: AM5746

I need to select the best processor for the following specification/Project Requirement:

Project Requirement
Processor ?
OS(Android/Linux)
Wifi Module
Bluetooth
Analog (12-16bit)
GPIO (4-8#)
RS232 & RS485
Programming and Debugging Capability
Touch Display(5.5in)
USB - A type(OTG)
GSM Interface
Battery Operated(Opr-8Hrs)

with regards,

Srinivasan M

  • Thanks for considering our Processors.

    You will need a Sitara Processor plus SimpleLink parts, since Sitara Processors do not have integrated WiFI/BT/GSM interface.

    In this forum I can recommend to you to look into AM335x and AM437x. There is no Android support from TI for these 2 devices.

    For SimpleLink, you will need to check their parts via website or their e2e forum.

    I hope it helps.