Other Parts Discussed in Thread: THS8200
Dear Champ,
I want to playback 720p video with DM355 EVM and display component output from THS8200 EVM.
I encounter 2 diffculty here :
1. I use decode demo in dvsdk (1.30.00.40) to decode a 720P video which I already converted to DM355 format , but not successful. I can convert a vga video (also converted to DM355 format. ) but not 720p.
How can I playback a HD video with DM355 EVM ?
My bootarg is
console=ttyS0,115200n8 noinitrd rw ip=$(ipaddr):::off root=/dev/nfs nfsroot=$(serverip):/home/user/workdir/filesys,nolock mem=116M
video=davincifb:vid0=1280x720x16,5529K:vid1=1280x720x16,5529K davinci_enc_mngr.ch0_output=COMPONENT1 davinci_enc_mngr.ch0_mode=720P-60
Should it be 720P_60 or 720P-60 ?
2. If I playback a vga video, I can get CLKIN (27Mhx) and Hsync (33Khz) and Vsync ( 65Hz ) and also some activity on the Y and C bus. So I think COMPONENT1 output is working and I can get digital output from EVM.
But how can I setup davinci_enc_mngr.ch0_mode for vga resolution ?
Can I setup davinci_enc_mngr.ch0_mode=640*480 and still have COMPONENT1 as my output and get THS8200 board working to display vga video ?
OR if I use COMPONENT1, I can only use 720P or 1080i unless I modify the display driver files ?
Pls help. I've been working on this problem for quite some time and still get stuck here.
Definitely need some help. Thks.