Part Number: TMS320C6748
I'm looking to config the PLL:
OSC Frequency: 20 MHz
CPU: 300 MHz
EMIFA: 100 MHz
DDR2: 200 MHz
I've installed Starterware. I don't see any examples (The example for GPIO works fine).
If someone could point me in the right direction that would be great.
Alan