This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error while running the program

Other Parts Discussed in Thread: CCSTUDIO

Dear sir / madam,

 

I am Dharshak, currently doing my Master's. I am working on a project based on image processing. The C code has been written to process the image(8x8 bitmap image only), and is error free. The same program has to be implemented on  a DSP kit TMS320C6713. There is a problem while simulating the C code in ccstudio. The following error is displayed when I include certain parts of the C code, and the same error doesn't occur when that part of the C program is  removed. The error is

U:   Memory Map Error: WRITE access by Default to address 0xfffffe60, which is RESERVED in Hardware.

I am using CCSTUDIO V3.1. Looking forward for your reply.

 

Thanking you,

DHARSHAK.B.S