Part Number: AM4378
Hi,
I have a VAR-SOM-AM43 Development Kit and I am following the instruction on the Variscite Wiki: VarWiki
Upon executing the following script:
MACHINE=varsomam43 bitbake tisdk-rootfs-image
I receive the following error:
caruban@SolarCrucible:~/yocto_varsomam43/tisdk/build$ . conf/setenv
caruban@SolarCrucible:~/yocto_varsomam43/tisdk/build$ export PATH=/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:$PATH
caruban@SolarCrucible:~/yocto_varsomam43/tisdk/build$ MACHINE=varsomam43 bitbake tisdk-rootfs-image
Parsing recipes: 100% |#######################################################################################################| Time: 00:04:15
Parsing of 2247 .bb files complete (0 cached, 2247 parsed). 2839 targets, 493 skipped, 1 masked, 0 errors.
WARNING: No recipes available for:
/home/caruban/yocto_varsomam43/tisdk/sources/meta-arago/meta-arago-distro/recipes-multimedia/libav/libav_9.16.bbappend
/home/caruban/yocto_varsomam43/tisdk/sources/meta-processor-sdk/recipes-core/udev/udev_182.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-18.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "varsomam43"
DISTRO = "arago"
DISTRO_VERSION = "2016.05"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard cortexa9"
TARGET_FPU = "hard"
meta-variscite-amx3 = "krogoth:a64a84e4764cccfb43ead1de4493939536c797fc"
meta-processor-sdk = "HEAD:1686d851985872f34ca3a2c30d4a0726a20a5c99"
meta-arago-distro
meta-arago-extras = "HEAD:36598b78a6d9fbe442f93111f64d3413c04418a8"
meta-qt5 = "HEAD:d715f2c1d340fa38f8a9860acc73de5e14a38b75"
meta-networking
meta-ruby
meta-python
meta-oe = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-ti = "HEAD:1ae0cadb1200d0007a779958e852a48379d42c26"
meta-linaro-toolchain = "HEAD:0f2a4dd08ab06768cc998fe3f7236e3942f4a2cc"
meta = "HEAD:b0b91490e4ede61a302eb547da2cc65aa7da87ff"
NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: gnu-config-native-20150728+gitAUTOINC+b576fa87c1-r0 do_unpack: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
fatal: the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead.
ERROR: Logfile of failure stored in: /home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/temp/log.do_unpack.6039
Log data follows:
| DEBUG: Executing python function do_unpack
| DEBUG: Executing python function base_do_unpack
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1487"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts/native-intercept:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/caruban"; git -c core.fsyncobjectfiles=0 clone -s -n /home/caruban/yocto_dl/git2/git.sv.gnu.org.config.git/ /home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/git/
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1487"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts/native-intercept:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/caruban"; git -c core.fsyncobjectfiles=0 remote set-url origin git://git.sv.gnu.org/config.git
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1487"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts/native-intercept:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/caruban"; git -c core.fsyncobjectfiles=0 checkout -B master b576fa87c140b824466ef1638e945e87dc5c0343
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1487"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts/native-intercept:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/caruban/yocto_varsomam43/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/scripts:/home/caruban/yocto_varsomam43/tisdk/sources/bitbake/bin:/opt/gcc-linaro-5.3.1-2016.05-x86_64_arm-linux-gnueabihf/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/caruban"; git -c core.fsyncobjectfiles=0 branch --set-upstream master origin/master
| DEBUG: Python function base_do_unpack finished
| DEBUG: Python function do_unpack finished
| ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
| fatal: the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead.
|
ERROR: Task 743 (virtual:native:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_unpack) failed with exit code '1'
NOTE: Tasks Summary: Attempted 10 tasks of which 7 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
virtual:native:/home/caruban/yocto_varsomam43/tisdk/sources/oe-core/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_unpack
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
It seems that a command is outdated with the current system I am using. I am running a Linux 18.04 LTS on the host PC.
Is there any way to fix this?
Kind regards,
Shoaib