Part Number: TMS320C6678
We are currently using a TMS320C6678ACYP in our application. At high ambient temperature we experience thermal runaway in the device. We have considered changing to the extended version of the device (TMS320C6678ACYPA) as it can handle higher case temperature. However, we want to make sure this will have a positive impact in our system. We are concerned about the following:
1) The current consumption is heavily dominated by baseline currents at high case temperature and these grow exponentially with temperature. The power calculation spreadsheet does not differentiate between the normal and the extended version, but does not allow ambient temperature to be set to 100C. Are the baseline currents equal for the normal and the extended temperature devices? If so, can we extrapolate the baseline currents to 100C? If we do so, the resulting baseline currents would be so high, that the power consumption in the device would be much higher than what has been recommend for the package in other threads in here. This seems like a paradox. What baseline current can be considered maximum for the extended version at 100C case temperature?
2) If the extended version does not have lower baseline power consumption, what causes it to handle 100C case temperature instead of 85C in the normal version.
Thanks,
Sigurd