Hello,
We have purchased the AM3517 Zoom Experimenters kit and I am trying to get basic WindowsCE demos to work.
Using the TI_SDCard_boot_utility I formatted a USB memory stick with EBOOTSD.nb0, MLO and NK_demo.bin.
I have not been able to figure out how boot from the USB memory stick. I press a key during X-Loader initialization to stop the boot from flash (which loads Arago Linux) and when I type USBBoot I get the message "No boot device". The USB Memory stick is plugged into the USB Host port on the eXperimenter BaseBoard.
Also if anyone has any help with Windows CE 7.0 that would be great. I downloaded CE 7.0 and built a 3530 OS image (thinking that it might run on the 3517, but I have no way of loading the NK.bin file to try it)
thank you,
-Reinyn