This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355 H3A issue!



I have already read  the document of spruf71a.pdf,  If H3A obtain RAW

data format images from the CCDC, and then write images  to the buffer

logic, then IPIPE read images from the buffer logic,after IPIPE 

processing ,raw data format make into YUV format. Finally, the image

display on the LCD screen. 
but H3A signal processing Flow is not very clear!
(1)Is there anything about H3A image processing flow chart?
(2)H3A input RAW DATA format,  whether output data format is raw data

format or YUV format after H3A processed?

any help and suggest would be an appreciate !