Part Number: TDA3LA
Hi team,
According to the following link: http://www.ti.com/processors/digital-signal-processors/libraries/c66x-video-codecs.html
1. Can I use 1 C66x core inside TDA3LA as a H.264 decoder at 480p30 resolution (High Profile)? The library requires 0.5 C66x core runing at 1.25GHz while the TDA2LA has 1 C66x core, max frequency is 745MHz.
2. What is the 480p resolution mentioned? 854 x 480 (16:9 480p) or 640 x 480 (4:3 480p) or?
3. Is 1 C66x possible to support up to 480p 60fps (High Profile)?
Thank you.
Kien