This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question regarding VPBE



Hi,

How does one access the VPBE?  Is there any documentation on how to do this, or an example?

Thanks

  • NeeravPatel said:

    How does one access the VPBE?  Is there any documentation on how to do this, or an example?

    Documentation on the VPBE for the DM355 can be found in the VPBE User's Guide (SPRUF72).

    An example using this interface would be available via the Linux LSP for the DM355.

  • To add to Brandon's response

    1) from a hardware perspective: VPBE UG is the place to look

    2) From a software driver perspective: the driver source code is located in two directories

         .../ti-davinci/drivers/media/video/davinci     (V4L2 driver)

        .../ti-davinci/drivers/video/davinci   (FBDev Driver)

    There is documentation included in the dvsdk_`_30_00_41/PSP_01_20_00_014 that describes these driver architectures.

    3) From a software application perspective, there are demos included in the dvsdk_1_30_00_41/demos/dm355 (includes source code) that show you how to use drivers