Other Parts Discussed in Thread: OMAP-L138
Hi,
I have come across 2 versions of this document "OMAP-L138 Low-Power Applications Processor".
The older version (SPRS586A–JUNE 2009–REVISED AUGUST 2009 ):
6.19 Universal Serial Bus OTG Controller (USB0) [USB2.0 OTG]
The USB2.0 peripheral supports the following features:
· USB 2.0 peripheral at speeds high speed (HS: 480 Mb/s - C6747 only) and full speed (FS: 12 Mb/s)
The newer version (SPRS586B – JUNE 2009 – REVISED AUGUST 2010):
6.20 Universal Serial Bus OTG Controller (USB0) [USB2.0 OTG]
The USB2.0 peripheral supports the following features:
• USB 2.0 peripheral at speeds high speed (HS: 480 Mb/s) and full speed (FS: 12 Mb/s)
The discrepancy bothers me. Would like to confirm, does ARM (OMAP L138) support high speed (480 Mb/s) USB ?
Our current project is relying on ARM to be the high speed USB device. If this is not the case, then OMAP L138 will not be suitable for the project anymore.
rgds,
kc Wong