This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM65X: GP EVM touchscreen issue

Part Number: PROCESSOR-SDK-AM65X


Hi

Now I get TMDX654GPEVM-TMDSLCD1EVM (http://www.tij.co.jp/tool/jp/TMDX654GPEVM) with SD card which includes SW already.

1. Boot the EVM with SD card

2. Succeed LINUX login as "root" on UART terminal

3. Only at first boot time, the screen "+ pointer image with white background " was appeared .

    However, I didn't anything.

    After that, I don't see this screen never.

4. Cannot select Desired icon

Is it because the touch panel calibration has failed?

What is the command to call the calibration by UART terminal?

Thanks and best regards,

HaTa.

How to execute