Hello,
I am trying to build OS and getting error when bitbake compiles intltool-native. Please check the log below:
Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-18.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "XXXX"
DISTRO = "arago"
DISTRO_VERSION = "2017.06"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:2b7f7b00654eb3faaea7c66271ebe508b9ffc019"
meta-arago-distro
meta-arago-extras = "HEAD:8f49ed67d0627a04ac72fd388fda7756273ba2d7"
meta-browser = "HEAD:08576b03af624b65ad949c410d84c11c7d1f2e39"
meta-openamp = "HEAD:8a214032bfb7e8124bc1485c70c69f7d60abb819"
meta-qt5 = "HEAD:2c9f0e4eb0e9097f6f872ec1e1d81768a8ab5f1b"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-ti = "HEAD:a18d57af8384ced25996739bb66d197c69efb77b"
meta-linaro-toolchain
meta-optee = "HEAD:49b0f32d7e955f250b0022d1b2f403f45a2c2d9c"
meta = "HEAD:e3911133ee9aad7cc3ae89faea80a097f6614fab"
meta-XXXX = "XXXX:d66683146e2967995aba8877ff2f5ada8efe3edd"
meta-java = "master:65bd3d6eaa6ae4e06f1c04efb493f448cf6d619b"
Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:04
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: intltool-native-0.51.0-r0 do_configure: autoreconf execution failed.
ERROR: intltool-native-0.51.0-r0 do_configure: Function failed: do_configure (log file is located at /media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/int
ltool-native/0.51.0-r0/temp/log.do_configure.23231)
ERROR: Logfile of failure stored in: /media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/intltool-native/0.51.0-r0/temp/log.do_configure.23231
Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: Executing shell function autotools_preconfigure
| DEBUG: Shell function autotools_preconfigure finished
| DEBUG: Executing python function autotools_copy_aclocals
| DEBUG: Considering setscene task: ['texinfo-dummy-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['autoconf-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['m4-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['autoconf-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['xz-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['libxml-parser-perl-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['pigz-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['libxml-parser-perl-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['expat-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['libxml-parser-perl-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['perl-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['libxml-parser-perl-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['gettext-minimal-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['xz-native', 'do_populate_sysroot']
| DEBUG: Considering setscene task: ['zlib-native', 'do_populate_sysroot']
| DEBUG: considering dependency: ['pigz-native', 'do_populate_sysroot']
| DEBUG: SITE files ['endian-little', 'common-linux', 'common-glibc', 'bit-64', 'x86_64-linux', 'common']
| DEBUG: Python function autotools_copy_aclocals finished
| DEBUG: Executing shell function do_configure
| NOTE: Executing ACLOCAL="aclocal --system-acdir=/media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/intltool-native/0.51.0-r0/aclocal-copy/ --automake-acd
ir=/media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/aclocal-1.16" autoreconf --verbose --install --force --exclude=autopoint -I /media/dmai
suria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/intltool-native/0.51.0-r0/intltool-0.51.0/
| ERROR: autoreconf execution failed.
| automake (GNU automake) 1.16.1
| Copyright (C) 2018 Free Software Foundation, Inc.
| License GPLv2+: GNU GPL version 2 or later <gnu.org/.../gpl-2.0.html>
| This is free software: you are free to change and redistribute it.
| There is NO WARRANTY, to the extent permitted by law.
|
| Written by Tom Tromey <tromey@redhat.com>
| and Alexandre Duret-Lutz <adl@gnu.org>.
| AUTOV is 1.16
| autoreconf: Entering directory `.'
| autoreconf: configure.ac: not using Gettext
| autoreconf: running: aclocal --system-acdir=/media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/intltool-native/0.51.0-r0/aclocal-copy/ --automake-acdir=/
media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/aclocal-1.16 -I /media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-too
lchain/work/x86_64-linux/intltool-native/0.51.0-r0/intltool-0.51.0/ --force
| Dumper.c: loadable library and perl binaries are mismatched (got handshake key 0xdb00080, needed 0xde00080)
| aclocal: error: echo failed with exit status: 1
| autoreconf: aclocal failed with exit status: 1
| WARNING: /media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/intltool-native/0.51.0-r0/temp/run.do_configure.23231:1 exit 1 from 'exit 1'
| ERROR: Function failed: do_configure (log file is located at /media/dmaisuria/Storage/rayBuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/intltool-native/0.51.0-r0/temp/log.do_con
figure.23231)
ERROR: Task (virtual:native:/media/dmaisuria/Storage/rayBuild/tisdk/sources/oe-core/meta/recipes-devtools/intltool/intltool_0.51.0.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 776 tasks of which 766 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
virtual:native:/media/dmaisuria/Storage/rayBuild/tisdk/sources/oe-core/meta/recipes-devtools/intltool/intltool_0.51.0.bb:do_configure
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
I recently upgraded my OS from Ubuntu 16.04 to 18.04.
Any help would be greatly appreciated.
Thanks,
Divyeshkumar