This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IE can not open NFS file system of DM368IPNC-IMX036




I bought your company's DM368IPNC-IMX036 product from seeddsp ,and now some of the problems encountered, may I ask how to solve, thank you.
I follow the "Users_Guide_IPNC_DM368_IMX036.pdf" (version is Release Version: 1.0.0 July 2010) installed some software codes, and then "make sysall", compiled after a number of documents are generated, then I active the DM368IPNC-imx036 with NFS, but I can not use the IE to browse the images, ah, what is the cause, and thank you? ? ? ? ? ? ? ?

 

============================================================

this is console printing:

DM36x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000008.
   DONE
Jumping to entry point at 0x81080000.

 DM368_IPNC_UBL_1.0.0

U-Boot 1.3.4 (Apr 20 2010 - 11:42:44) DM368-IPNC-1.0.0

I2C:   ready
DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Bad block table found at page 65472, version 0x01
Bad block table found at page 65408, version 0x01
128 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 432MHz
DDR Clock :- 340MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot:  0
DM368 IPNC :>setenv ipaddr 192.168.1.168;setenv serverip 192.168.1.234;setenv ethaddr 00:0C:0C:A0:05:cb;setenv bootcmd 'tftpboot 0x80700000 uImage_ipnc_DM368_IMX036-nfs; bootm 0x80700000';setenv bootargs console=ttyS1,115200n8 noinitrd rw ip=192.168.1.168:192.168.1.167:192.168.1.1:255.255.255.0:::off eth=00:0C:0C:A0:05:cb root=/dev/nfs nfsroot=192.168.1.234:/opt/ip368cam/ipnc/target/filesys,nolock mem=48M;boot
TFTP from server 192.168.1.234; our IP address is 192.168.1.168
Filename 'uImage_ipnc_DM368_IMX036-nfs'.
Load address: 0x80700000
Loading: #################################################################
         ###############################################################
done
Bytes transferred = 1870452 (1c8a74 hex)
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1870388 Bytes =  1.8 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.0.0 (root@localhost.localdomain) (gcc 版本 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Tue Dec 14 09:58:35 CST 2010
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM368 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000
PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428
PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 12288
Kernel command line: console=ttyS1,115200n8 noinitrd rw ip=192.168.1.168:192.168.1.167:192.168.1.1:255.255.255.0:::off eth=00:0C:0C:A0:05:cb root=/dev/nfs nfsroot=192.168.1.234:/opt/ip368cam/ipnc/target/filesys,nolock mem=48M
TI DaVinci EMAC: kernel boot params Ethernet address: 00:0C:0C:A0:05:cb
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 48MB = 48MB total
Memory: 44568KB available (3205K code, 654K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered

 ***davinci_spi_board_init()!<6>
 ***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Dec 14 2010 09:55:06 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is 00:0C:0C:A0:05:cb
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
Trying to register davinci display video device.
layer=c0653000,layer->video_dev=c0653160
Trying to register davinci display video device.
layer=c0630e00,layer->video_dev=c0630f60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Creating 7 MTD partitions on "nand_davinci.0":
0x00000000-0x00300000 : "bootloader"
0x00300000-0x00500000 : "params"
0x00500000-0x00700000 : "kernel"
0x00700000-0x02700000 : "filesystem"
0x02700000-0x02900000 : "data1"
0x02900000-0x02d00000 : "Calibration"
0x02d00000-0x08000000 : "data2"
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
dm_spi.0: davinci SPI Controller driver at 0xc3866000 (irq = 42) use_dma=0
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Peripheral mode controller at c3868000 using DMA, IRQ 12
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
  #0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 00:53:42 (946688022)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
IP-Config: Complete:
      device=eth0, addr=192.168.1.168, mask=255.255.255.0, gw=192.168.1.1,
     host=192.168.1.168, domain=, nis-domain=(none),
     bootserver=192.168.1.167, rootserver=192.168.1.234, rootpath=
Looking up port of RPC 100003/2 on 192.168.1.234
Looking up port of RPC 100005/1 on 192.168.1.234
VFS: Mounted root (nfs filesystem).
Freeing init memory: 184K
INIT: version 2.86 booting
0
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
0
CSL: Module install successful, device major num = 253
CSL: Module version 0.10.00, built on Dec 14 2010 10:01:15
I2C: Module install successful, device major num = 252
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Dec 14 2010 10:01:18
DRV: EDMACC.QUEPRI  = 00000777
DRV: SYSTEM.MSTPRI0 = 00550011
DRV: SYSTEM.MSTPRI1 = 00000444
DRV: ISP.BCR        = 00000002
DRV: SYSTEM.MISC = 00000391
CMEMK module: built on Dec 14 2010 at 10:00:37
  Reference Linux version 2.6.18
  File /opt/ip368cam/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
allocated heap buffer 0xc4000000 of size 0x4e00000
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83000000)
cmemk initialized
EDMAK module: built on Dec 14 2010 at 10:00:40
  Reference Linux version 2.6.18
  File /opt/ip368cam/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c
IRQK module: built on Dec 14 2010 at 10:00:42
  Reference Linux version 2.6.18
  File /opt/ip368cam/dvsdk_2_10_01_18/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c
irqk initialized
=========starting system_server================
Creat queue id:0
queue id:0
FileMngThread created
Creat queue id:32769
queue id:32769
AlramThread created
Share memory init success
IPNC_DM368_2.0.0 (root@localhost.localdomain) (gcc
版本 4.2.0
Creat queue id:65538
queue id:65538
queue id:32769
queue id:65538

CPU is DM368
DEMOCFG Value   : 0
Videocodecmode  : 0
Videocodecres   : 0
Starting mounting local filesystems: mount none on /dev/shm type tmpfs (rw,size=5M)
none on /var/run type tmpfs (rw)
none on /tmp type tmpfs (rw,sync)
Setting up networking ....
Starting hotplug subsystem:
   pci    
   pci      [success]
   usb    
   usb      [success]
   isapnp 
   isapnp   [success]
   ide    
   ide      [success]
   input  
   input    [success]
   scsi   
   scsi     [success]
done.
Starting portmap daemon: portmap.
Starting internet superserver: inetd.
io scheduler deadline registered
io scheduler cfq registered
insmod: /opt/ipnc/modules/i2c-emac.ko: No such file or directory
 sbulla: unknown partition table
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
loop: loaded (max 8 devices)
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CSLIP: code copyright 1989 Regents of the University of California
PPP generic driver version 2.4.2
insmod: /opt/ipnc/modules/netconsole.ko: No such file or directory
PPP Deflate Compression module registered
insmod: /opt/ipnc/modules/davinci_emac.ko: No such file or directory
insmod: /opt/ipnc/modules/mmc_core.ko: No such file or directory
insmod: /opt/ipnc/modules/mmc_block.ko: No such file or directory
insmod: /opt/ipnc/modules/davinci-mmc.ko: No such file or directory
insmod: /opt/ipnc/modules/usbcore.ko: No such file or directory
insmod: /opt/ipnc/modules/musb_hdrc.ko: No such file or directory
insmod: /opt/ipnc/modules/usbmon.ko: No such file or directory
Loading iSCSI transport class v1.1-646.<5>iscsi: registered transport (tcp)
 sbulla: unknown partition table
mkdosfs 3.0.6 (04 Oct 2009)
unable to get drive geometry, using default 255/63
/dev/sbulla has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 1024 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 1 sector, and provides 247 clusters.
Root directory contains 512 slots.
Volume ID is 02b5911e, no volume label.
queue id:0
TimeOut occure in boot_proc.
Program exit.
ApproDrvInit: 3
Creat queue id:98307
queue id:98307
INIT: Entering runlevel: 3

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)

192.168.1.168 login: