Part Number: TMS320DM8147
Other Parts Discussed in Thread: CCSTUDIO
We have noticed that the 814x u-boot is manipulating registers that don't seem to be documented in the TRM
For instance the following is defined in u-boot-omap3\arch\arm\include\asm\arch-ti81xx\cpu.h
Line 427: #define CM_DEFAULT_L3_FAST_CLKSTCTRL (PRCM_BASE + 0x0508)
and u-boot has code that does things like (in ddr2.c):
/*Enable the Power Domain Transition of L3 Fast Domain Peripheral */
__raw_writel(0x2, CM_DEFAULT_L3_FAST_CLKSTCTRL);
However, the TRM documents only a subset of these. See section 2.10.7
Is the u-boot code incorrect?. Or is the TRM incorrect?
thanks