This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6657: EMIF16 Brig-up an .gel file

Part Number: TMS320C6657


Tool/software: Code Composer Studio

Good Morining,

I need to modify the evmc6657l.gel file from the Evaluation Board in order to support EMIF16 access.

I tried adding statements to configure:

1. PIN_CONTROL_1 register at address 0x02620580;

2. AxCR register at address 0x20C0001x;

But  unfortunally with an oscilloscope probe I don't see the nEMIFCEx to move when I visualize the memory space at address 0x7x000000.

Are there any other register to set in order to perform an EMIF16 Access from the Code Composer Studio through an emulator?

Could someone give an example?

Thanks in advance

Regards