Hello 36x gurus,
I have a question about the EMIF interface clock cycle as two documents seem to be in conflict:
1) EMIF users guide SPRUFI1C – page 46 – says tCYC is the period at which the EMIF operates. This value is used in all the setup, strobe and hold calculations in that document.
2) DM365 datasheet SPRS457D – page 101 – says E=(0.5)*PLLC1 SYSCLK4 period in ns. This value is used in all the setup, strobe and hold calculations in that document.
Our SYSCLK4 is 121.5MHz (8.23ns)
E = 0.5 * 8.23ns = 4.12ns
I believe that tCYC and E are the same but this is where I need confirmation. Is tCYC 8.23ns or is it 4.12ns?
Thanks,
Katie