Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138
I installed ti-processor-sdk-rtos-omapl138-lcdk-06.00.07-Windows-x86-Install.exe, but no PDK samples are created.
CCS9.1 (CCS9.1.0.00010_win64.zip) is installed in C:TI.
Processor-SDK-ti-processor-sdk-rtos-omapl138-lcdk-06.00.00.07-Windows-x86-Install.exe_ is installed in the default folder.
ruRun pdksetup.bat at c:tipdk_omapl138_1_0_9packages.n setupenv.bat at c:tiprocessor_sdk_rtos_omapl138_6_00_00_07.
OmaPL138 environment specified.
run gmake all at c:tipdk_omapl138_1_0_9packages.
(You've already done it several times.) Log 483 lines)
run pdkProjectCreate.bat with c:tipdk_omapl138_1_0_9packages.
PDK_PARTNO : OMAPL138
PDK_ECLIPSE_ID : com.ti.pdk.omapl138
RTSC_PLATFORM_NAME : ti.platforms.evmOMAPL138
RTSC_TARGET : ti.targets.arm.elf.Arm9 CCS_DEVICE : "ARM9.
OMAPL138"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace c:tiPDK_OM~1packagesMyExampleProjects
Detected Test Project: EMAC_lcdkOMAPL138_ARMLoopback_testProject
The specified path cannot be found.
Copying macro.ini
The specified path cannot be found.
You have copied 0 files.
Detected Test Project: GPIO_LedBlink_lcdkOMAPL138_armTestProject
The specified path cannot be found.
Copying macro.ini
The specified path cannot be found. You have copied 0 files.
An error occurs when the path is not found.
What caused the error?