This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NetworkRx to Isp

I have created a usecase which have 

networkRx(A15)-> IssM2mIsp-> Display

Issm2miisp->Alg_aewb.

When i am running the usecase  i am getting the following error.

Launch HM Test: network isp display....
[IPU1-0] 19.782559 s: Chains: Using TCP/IP
[IPU1-0] 20.790184 s: IPC_IN_0 : Create in progress !!!
[IPU1-0] 20.791221 s: IPC_IN_0 : Create Done !!!
[IPU1-0] 20.791374 s: ISSM2MISP: Create in progress !!!
[IPU1-0] 20.953608 s: UTILS: DMA: Allocated CH (TCC) = 48 (48)
[IPU1-0] 20.953730 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 48 (0x63304800)
[IPU1-0] 20.957725 s: 7835: Assertion @ Line: 1234 in isscore/src/vpscore_ispapi.c: FALSE : failed !!!
[HOST ] 20.789940 s: NETWORK_RX: NETWORK_RX: Server listening (port=29171) !!!
[HOST ] 20.790062 s: IPC_OUT_0 : Create in progress !!!
[HOST ] 20.790093 s: IPC_OUT_0 : Create Done !!!
[HOST ] 21.003141 s: NDK: Link Status: 1000Mb/s Full Duplex on PHY 2

Please help in solving this error.

Thanks and regards,

Aneesh