Part Number: AM3354
Hi,
I would like to add multiple CS (Chip Select) support in the device tree to handle multiple SPI devices with help of /dev/spidev1.x (x is a number of CS) nodes. Please find below snippet of my device tree.
spi1_pins: pinmux_spi1_pins {
pinctrl-single,pins = <
0x190 (PIN_INPUT_PULLUP | MUX_MODE3) /* mcasp0_aclkx.spi1_sclk */
0x194 (PIN_INPUT_PULLUP | MUX_MODE3) /* mcasp0_fsx.spi1_d0 */
0x198 (PIN_INPUT_PULLUP | MUX_MODE3) /* mcasp0_axr0.spi1_d1 */
0x19C (PIN_INPUT_PULLUP | MUX_MODE3) /* mcasp0_ahclkr.spi1_cs0 */
0x108 (MUX_MODE7) /* mii1_col.gpio3_0 */
>;
};
&spi1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi1_pins>;
ti,pindir-d0-out-d1-in = <1>;
spidev@0 {
compatible = "linux,spidev";
spi-max-frequency = <20000000>;
reg = <0>;
};
spidev@1 {
compatible = "linux,spidev";
spi-max-frequency = <20000000>;
reg = <1>;
};
};
With the mentioned device tree information, I am only able to handle spidev1.0 with the CS0 pin. I am not able to handle spidev1.1 with the CS1 pin. Kindly help me to resolve this issue.
Best Regards,
Neel