Hi,
In TMS320C6652CZHA6 I need clarifications on the below
1. MCIMCLKP / N
I am not using MCIM in the design. These pins are mentioned are reserved in datasheet.Can these pins be left floating.
2.GPIO pins
Should we add pullup/pull down on GPIO input pins? I understand from datasheet GPIO outputs doesnot require pullup/down.
Also series termination to be used on GPIO outputs. Please confirm.
3. MDCLK
MDC is not used in the design. Can this pin be left floating?
Thanks,
Divy